自己在helloworld的例程上稍微改动了一下,运行时提示:
[C66xx_0]
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
TCP/IP Stack 'Hello World!' Application
TCP/IP Stack 'Hello World!' Application
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Network Added: If-1:192.168.0.234
我使用的是SGMII0 PHY模式,通过查看SGMII_CONTROL STATUS MR_ADV_ABILITY三个寄存器值为:00000001 0000003D 00001801,我看了一下这几个寄存器的值也应该正确,但是我和PC机 就是ping不通,请问大家有遇见这种情况的吗?怎么解决的?