This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168挂载固态硬盘SSD的问题,驱动支持吗?



亲们,今天在对固态硬盘进行分区的时候,小的2G的分区sda2,能正常格式化,大一点的分区950G的sda1格式化就是老是提示出错,分区使用的命令是:

mkfs.ext3 -c /dev/sda 也用过mkfs.ext3  /dev/sda 效果从差不多

格式950G分区出现的错误如下:

end_request: I/O error, dev sda, sector 64
sd 0:0:0:0: [sda] Unhandled error code
sd 0:0:0:0: [sda]  Result: hostbyte=0x04 driverbyte=0x00
sd 0:0:0:0: [sda] CDB: cdb[0]=0x28: 28 00 00 00 00 40 00 00 08 00
end_request: I/O error, dev sda, sector 64
sd 0:0:0:0: [sda] Unhandled error code
sd 0:0:0:0: [sda]  Result: hostbyte=0x04 driverbyte=0x00
sd 0:0:0:0: [sda] CDB: cdb[0]=0x28: 28 00 00 00 01 00 00 00 08 00
end_request: I/O error, dev sda, sector 256
sd 0:0:0:0: [sda] Unhandled error code
sd 0:0:0:0: [sda]  Result: hostbyte=0x04 driverbyte=0x00
sd 0:0:0:0: [sda] CDB: cdb[0]=0x28: 28 00 00 00 00 00 00 00 08 00
end_request: I/O error, dev sda, sector 0
sd 0:0:0:0: [sda] Unhandled error code
sd 0:0:0:0: [sda]  Result: hostbyte=0x04 driverbyte=0x00
sd 0:0:0:0: [sda] CDB: cdb[0]=0x28: 28 00 00 00 00 00 00 00 08 00
end_request: I/O error, dev sda, sector 0
sd 0:0:0:0: [sda] Unhandled error code
sd 0:0:0:0: [sda]  Result: hostbyte=0x04 driverbyte=0x00
sd 0:0:0:0: [sda] CDB: cdb[0]=0x28: 28 00 00 00 00 00 00 00 08 00
end_request: I/O error, dev sda, sector 0
sd 0:0:0:0: [sda] Unhandled error code
sd 0:0:0:0: [sda]  Result: hostbyte=0x04 driverbyte=0x00
sd 0:0:0:0: [sda] CDB: cdb[0]=0x28: 28 00 00 00 00 00 00 00 08 00
end_request: I/O error, dev sda, sector 0
sd 0:0:0:0: [sda] Unhandled error code
sd 0:0:0:0: [sda]  Result: hostbyte=0x04 driverbyte=0x00
sd 0:0:0:0: [sda] CDB: cdb[0]=0x28: 28 00 00 00 00 00 00 00 08 00 

看提示好像都是driverbyte=0x00的问题,是固态硬盘驱动不支持吗?

我在http://processors.wiki.ti.com/index.php/TI_SATA_FAQ#Debugging_TIPS  这里看到下面的几句话

Name some devices that could be connected to a SATA interface

SATA interface could be used to connect following devices. Please note that these devices should have SATA/eSATA connector at their end.

  • HDD
  • CD/DVD drives
  • S/W RAID
  • External RAID storage towers
  • Solid State Devices
  • Port Multiplier
  • Port Selector
  • Blu-Ray

From the above list what are the devices validated with our EVMs

  • HDD
  • CD/DVD drives. Both laptop and external form-factors
  • External RAID Storage towers [Only as a device no configuration support. Vendor provided tool should be used on x86 Linux, Windows machine to configure RAID]
  • Port Multiplier

也就是说只有HDD ,CD/DVD,External RAID Storage towers,Port Multiplier对于EVMs是有效的,难道固态硬盘SSD驱动支持不了吗?谢谢~