This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMC6678L,利用Helloworld例程将DSP和ARM通信问题



目前已经可以利用Helloworld例程与PC进行UDP通信,目前遇到问题如下:

1,目前能利用DSP能收到ARM发送过来的UDP包,但是DSP利用sendto函数发送接收到的UDP

包,ARM无法收到。目前测试DSP与ARM分别于PC进行通信正常,但是ARM就是接不到DSP发出的UDP包。端口,IP设置都没有问题。

2,将TCP替换UDP程序,无法利用TCP与PC通信,出现的问题是堆栈溢出(我修改过堆栈,但是没什么作用)

请教一下各位,谢谢了!(CCS5.2版本,Mcsdk_2_01_02_06)