This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 VPIF接口采集,如何配置实用外同步信号

Other Parts Discussed in Thread: TVP5158, TVP7002

你好。

由于实用的是dm6467t dvsdk3.0的开发平台,使用的采集芯片是tvp5158 进行解码,直接通过16bit的数据线连接到dm6467t端,采用的是内同步,即判断sav2eav、eav2sav 来确定图像帧。

  目前输入的信号时1024x768@60hz ,解码芯片是adv7441。现在想使用外同步即hs 和vs连接到dm6467t的vpif端,以前的vpif_cupture.c 以及相关配置需要如何修改?vpif中的配置参数都是和eav和sav相关的,现在不知道与外同步的如何配置?谢谢!