因为设计原理图时的疏忽,送给C6678的时钟,在板子通电后即有效,而且一直有效,不能接受FPGA的控制,没有仿照evm板的时钟设计,请问这会影响之后DSP上电的有效性和稳定性吗?因为看文档的介绍,好像时钟要在核电压、1.0V、1.8V有效之后才能有效。
但通过测试,我的设计即使时钟一直有效,上电之后,c6678的resetstat*信号状态可以返回1,证明上电有效呀。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为设计原理图时的疏忽,送给C6678的时钟,在板子通电后即有效,而且一直有效,不能接受FPGA的控制,没有仿照evm板的时钟设计,请问这会影响之后DSP上电的有效性和稳定性吗?因为看文档的介绍,好像时钟要在核电压、1.0V、1.8V有效之后才能有效。
但通过测试,我的设计即使时钟一直有效,上电之后,c6678的resetstat*信号状态可以返回1,证明上电有效呀。
谢谢。
没有,我就使用了一个普通lvds的100Mhz晶振直接送给DSPcore clock;使用了一个普通的lvds的62.5Mhz晶振直接送给DSP ddr clock。
通电就会产生3v3电压,送给这两个晶振,因此就会令时钟一直有效。
从时序图上的说明看,好像这两个时钟一直有效是允许的,请高手确认!谢谢。