This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:有关DM368 UARTBOOT加载速度的疑问



大家好,

    背景:我目前在使用DM368的UART BOOT加载版本,现在DM368基于24MHz晶振,通过实验发现,能够比较好的分频出来的波特率最高就是115200.

   需求:但是我们的版本比较大,大约10MB,这样加载下来十几分钟了。调试很不方便。

    硬件限制,也没有网口。

   想法:现在的想法是如何提升串口的波特率,但是试了一些方法都无效。

   1.直接设置为230400,这是因为计算分分频因子7与理论的分频因子6.5误差太大,无法正常工作。

  2.本来看UART支持13x分频,但发现这个只是一个只读的配置。只能使用16X,无法使用13x。

  3.UART0的时钟源是晶振,24MHz。

请各位了解UART BOOT加载的帮忙看看,还有什么办法。

谢谢了~~