This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM648通过profile->clock查看时间



TI你好:

我通过CCS3.3 profile->clock查看程序运行时间,通过仿真器查看,运行指令周期数显示480525915,CPU频率900MHZ,指令周期1.11ns,则程序运行时间大概为540ms,但是通过跑断点运行,感觉过了2-3秒钟才运行完,与profile->clock计算得到的540ms不太相符,请问是怎么回事呢?实际运行时间是按照540ms还是按照实际感觉到的时间?谢谢

  • c6000系列的dsp,不能使用CCS提供的profile工具来计算运行时间的

  • 请问一下,你的DM648的视频采集和显示能正常显示吗?我用C:\dvsdk_1_11_00_00_DM648\examples\video_preview\evmDM648下面的video_preview.c但是程序挂在FVID_dequeue(disChan, &frameBuffPtr)它是从dischan取出一个空闲的buffer当做整个采集显示循环的起始buffer,但是就是不明白FVID_dequeue函数是从qOut链上取的,但是前面分配的buffer都是挂在qIn上面,所以qOut是空链。既然库文件这么写的应该不会有问题,所以不知道我这边到底是硬件还是哪里出错了。