This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 DUP资源扩张问题

Other Parts Discussed in Thread: SYSBIOS

当修改#define DUP_LINK_OBJ_MAX   (4)到#define DUP_LINK_OBJ_MAX   (8)时,编译出现如下错误,如何解决:

"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/mcfw/src_bios6/cfg/ti816x/link_algs.cmd", line 12: warning:
   no matching section
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 239: error:
   placement fails for object ".const", size 0x1f0e3 (page 0).  Available
   ranges:
   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 241: error:
   placement fails for object ".fardata", size 0x30aa (page 0).  Available
   ranges:
   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 229: error:
   run placement fails for object ".stack", size 0x4000 (page 0).  Available
   ranges:
   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 250: error:
   placement fails for object ".vecs", size 0x5ff (page 0).  Available ranges:

   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 254: error:
   placement fails for object "ti_sdo_ipc_init", size 0x44b (page 0).
   Available ranges:
   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 246: error:
   placement fails for object ".cio", size 0x3c2 (page 0).  Available ranges:
   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 242: error:
   placement fails for object ".switch", size 0x32a (page 0).  Available
   ranges:
   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
"/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/obj/ti816x-evm/c6xdsp/debug/dvr_rdk_configuro/linker_mod.cmd", line 230: error:
   placement fails for object "GROUP_1", size 0x13c (page 0).  Available
   ranges:
   DDR3_DSP     size: 0xd80000     unused: 0xc          max hole: 0x4       
warning: entry-point symbol other than "_c_int00" specified:
   "ti_sysbios_family_c64p_Hwi0"
error: errors encountered during linking;
   "/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/bin/ti816x
   -evm/dvr_rdk_c6xdsp_debug.xe674" not built
make[3]: *** [/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/../dvr_rdk/build/dvr_rdk/bin/ti816x-evm/dvr_rdk_c6xdsp_debug.xe674] 错误 1
make[3]: Leaving directory `/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/mcfw/src_bios6/main_app'
make[2]: *** [apps] 错误 2
make[2]: Leaving directory `/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk/mcfw/src_bios6'
make[1]: *** [dvr_rdk_bios6] 错误 2
make[1]: Leaving directory `/home/liuhb/liuhb/MCU_CARD_V3.0/dvr_rdk'
make: *** [sdk-build] 错误 2
[root@localhost product]#

x 出现错误。请重试或与管理员联系。