Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 3.14.43-g875c69b (jinda@ubuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #1 Wed Oct 7 22:15:39 PDT 2015
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM-SK
[ 0.000000] cma: CMA: reserved 24 MiB at 8c800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES1.0 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64768
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 225284K/261120K available (5843K kernel code, 303K rwdata, 2144K rodata, 260K init, 232K bss, 35836K reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff000000 ( 744 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc07d50c4 (7989 kB)
[ 0.000000] .init : 0xc07d6000 - 0xc0817144 ( 261 kB)
[ 0.000000] .data : 0xc0818000 - 0xc0863da0 ( 304 kB)
[ 0.000000] .bss : 0xc0863da0 - 0xc089ddb8 ( 233 kB)
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956969942ns
[ 0.000038] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000332] Console: colour dummy device 80x30
[ 0.000359] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000366] This ensures that you still see kernel messages. Please
[ 0.000371] update your kernel commandline.
[ 0.000395] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.119362] pid_max: default: 32768 minimum: 301
[ 0.119466] Security Framework initialized
[ 0.119525] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119538] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.127611] CPU: Testing write buffer coherency: ok
[ 0.128024] Setting up static identity map for 0x805baa20 - 0x805baa78
[ 0.129054] devtmpfs: initialized
[ 0.131085] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.138977] omap_hwmod: tptc0 using broken dt data from edma
[ 0.139066] omap_hwmod: tptc1 using broken dt data from edma
[ 0.139146] omap_hwmod: tptc2 using broken dt data from edma
[ 0.143532] omap_hwmod: debugss: _wait_target_disable failed
[ 0.199500] pinctrl core: initialized pinctrl subsystem
[ 0.200604] regulator-dummy: no parameters
[ 0.203076] NET: Registered protocol family 16
[ 0.205231] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.207985] cpuidle: using governor ladder
[ 0.208003] cpuidle: using governor menu
[ 0.215026] syscon 44e10000.control_module: regmap [mem 0x44e10000-0x44e107fb] registered
[ 0.216601] platform 49000000.edma: alias fck already exists
[ 0.216626] platform 49000000.edma: alias fck already exists
[ 0.216642] platform 49000000.edma: alias fck already exists
[ 0.217862] OMAP GPIO hardware version 0.1
[ 0.233370] No ATAGs?
[ 0.233397] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.262263] bio: create slab <bio-0> at 0
[ 0.279779] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.280877] vbat: 5000 mV
[ 0.281304] lis3_reg: no parameters
[ 0.281416] reg-fixed-voltage fixedregulator@2: could not find pctldev for node /pinmux@44e10800/pinmux_wl12xx_gpio, deferring probe
[ 0.281442] platform fixedregulator@2: Driver reg-fixed-voltage requests probe deferral
[ 0.281919] vtt: 1500 mV
[ 0.285321] vgaarb: loaded
[ 0.285892] i2c-core: driver [palmas] using legacy suspend method
[ 0.285902] i2c-core: driver [palmas] using legacy resume method
[ 0.286686] SCSI subsystem initialized
[ 0.288284] usbcore: registered new interface driver usbfs
[ 0.288482] usbcore: registered new interface driver hub
[ 0.288704] usbcore: registered new device driver usb
[ 0.289816] omap_i2c 44e0b000.i2c: could not find pctldev for node /pinmux@44e10800/pinmux_i2c0_pins, deferring probe
[ 0.289849] platform 44e0b000.i2c: Driver omap_i2c requests probe deferral
[ 0.290290] pps_core: LinuxPPS API ver. 1 registered
[ 0.290301] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.290438] PTP clock support registered
[ 0.292553] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.293520] Advanced Linux Sound Architecture Driver Initialized.
[ 0.295265] Switched to clocksource timer1
[ 0.316584] NET: Registered protocol family 2
[ 0.317501] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.317539] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.317570] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.317639] TCP: reno registered
[ 0.317653] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.317673] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.317857] NET: Registered protocol family 1
[ 0.318281] RPC: Registered named UNIX socket transport module.
[ 0.318294] RPC: Registered udp transport module.
[ 0.318301] RPC: Registered tcp transport module.
[ 0.318308] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.319458] hw perfevents: enabled with ARMv7 Cortex-A8 PMU driver, 5 counters available
[ 0.322391] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.508776] VFS: Disk quotas dquot_6.5.2
[ 0.508849] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.509409] NFS: Registering the id_resolver key type
[ 0.509489] Key type id_resolver registered
[ 0.509498] Key type id_legacy registered
[ 0.509540] jffs2: version 2.2. (NAND) (SUMMARY) 漏 2001-2006 Red Hat, Inc.
[ 0.509733] msgmni has been set to 488
[ 0.511298] NET: Registered protocol family 38
[ 0.511343] io scheduler noop registered
[ 0.511351] io scheduler deadline registered
[ 0.511374] io scheduler cfq registered (default)
[ 0.513296] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.517558] backlight supply power not found, using dummy regulator
[ 0.521556] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.527394] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 88, base_baud = 3000000) is a 8250
[ 1.181231] console [ttyS0] enabled
[ 1.186787] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 1.193844] [drm] Initialized drm 1.1.0 20060810
[ 1.210251] brd: module loaded
[ 1.219455] loop: module loaded
[ 1.223036] (hci_tty): inside hci_tty_init
[ 1.227736] (hci_tty): allocated 250, 0
[ 1.236209] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.246909] usbcore: registered new interface driver asix
[ 1.252572] usbcore: registered new interface driver ax88179_178a
[ 1.258898] usbcore: registered new interface driver cdc_ether
[ 1.264986] usbcore: registered new interface driver smsc95xx
[ 1.270934] usbcore: registered new interface driver net1080
[ 1.276818] usbcore: registered new interface driver cdc_subset
[ 1.282952] usbcore: registered new interface driver zaurus
[ 1.288785] usbcore: registered new interface driver cdc_ncm
[ 1.295054] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.301649] ehci-pci: EHCI PCI platform driver
[ 1.306342] ehci-omap: OMAP-EHCI Host Controller driver
[ 1.312100] usbcore: registered new interface driver cdc_wdm
[ 1.318039] usbcore: registered new interface driver usb-storage
[ 1.325207] mousedev: PS/2 mouse device common for all mice
[ 1.332703] input: ti-tsc as /devices/ocp/44e0d000.tscadc/TI-am335x-tsc/input/input0
[ 1.342052] i2c-core: driver [rtc-ds1307] using legacy suspend method
[ 1.348570] i2c-core: driver [rtc-ds1307] using legacy resume method
[ 1.355841] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 1.362959] 44e3e000.rtc: already running
[ 1.367913] i2c /dev entries driver
[ 1.371608] Driver for 1-wire Dallas network protocol.
[ 1.379482] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.388579] omap_hsmmc 48060000.mmc: unable to get vmmc regulator -517
[ 1.395441] platform 48060000.mmc: Driver omap_hsmmc requests probe deferral
[ 1.402873] omap_hsmmc 481d8000.mmc: unable to get vmmc regulator -517
[ 1.409544] platform 481d8000.mmc: Driver omap_hsmmc requests probe deferral
[ 1.418988] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.425453] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 1.432601] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 1.440079] usbcore: registered new interface driver usbhid
[ 1.445716] usbhid: USB HID core driver
[ 1.449874] platform 44d00000.wkup_m3: Driver wkup_m3 requests probe deferral
[ 1.460500] oprofile: using arm/armv7
[ 1.464512] TCP: cubic registered
[ 1.467907] Initializing XFRM netlink socket
[ 1.472291] NET: Registered protocol family 17
[ 1.476847] NET: Registered protocol family 15
[ 1.481428] Key type dns_resolver registered
[ 1.486504] cpu cpu0: of_pm_voltdm_notifier_register: Failed to get cpu0 regulator/voltdm: -517
[ 1.495252] cpu cpu0: cpu0 clock notifier not ready, retry
[ 1.500909] platform cpufreq-cpu0.0: Driver cpufreq-cpu0 requests probe deferral
[ 1.509064] PM: bootloader does not support rtc-only!
[ 1.514152] ThumbEE CPU extension supported.
[ 1.518590] Registering SWP/SWPB emulation handler
[ 1.525101] lis3_reg: disabling
[ 1.528389] vbat: disabling
[ 1.531197] regulator-dummy: disabling
[ 1.535744] Error: Driver 'tfp410' is already registered, aborting...
[ 1.544791] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.551505] [drm] No driver support for vblank timestamp query.
[ 1.607805] Console: switching to colour frame buffer device 60x34
[ 1.616405] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.622004] tilcdc 4830e000.lcdc: registered panic notifier
[ 1.627635] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.634758] vwl1271: 1800 mV
[ 1.639912] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.650406] vrtc: 1800 mV
[ 1.653424] vrtc: supplied by vbat
[ 1.658663] vio: at 1500 mV
[ 1.661645] vio: supplied by vbat
[ 1.666874] vdd_mpu: 912 <--> 1375 mV at 1137 mV
[ 1.671677] vdd_mpu: supplied by vbat
[ 1.677240] vdd_core: 912 <--> 1150 mV at 1137 mV
[ 1.682144] vdd_core: supplied by vbat
[ 1.687339] vdd3: 5000 mV
[ 1.691471] vdig1: at 1800 mV
[ 1.694626] vdig1: supplied by vbat
[ 1.699589] vdig2: at 1800 mV
[ 1.702729] vdig2: supplied by vbat
[ 1.707682] vpll: at 1800 mV
[ 1.710742] vpll: supplied by vbat
[ 1.715631] vdac: at 1800 mV
[ 1.718694] vdac: supplied by vbat
[ 1.723503] vaux1: at 1800 mV
[ 1.726683] vaux1: supplied by vbat
[ 1.731631] vaux2: at 3300 mV
[ 1.734786] vaux2: supplied by vbat
[ 1.739740] vaux33: at 3300 mV
[ 1.742970] vaux33: supplied by vbat
[ 1.747969] vmmc: 1800 <--> 3300 mV at 3300 mV
[ 1.752593] vmmc: supplied by vbat
[ 1.757973] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.882584] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.892897] mmc0: new high speed SDHC card at address aaaa
[ 1.899087] mmcblk0: mmc0:aaaa SU04G 3.69 GiB
[ 1.905217] mmcblk0: p1 p2 p3
[ 1.926058] remoteproc0: wkup_m3 is available
[ 1.930537] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 1.939588] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 1.950212] remoteproc0: Direct firmware load failed with error -2
[ 1.956588] remoteproc0: Falling back to user helper
[ 1.962184] cpu cpu0: of_pm_voltdm_notifier_register: Fail calculating voltage latency[1100000<->1260000]:-22
[ 1.977619] omap_hsmmc 481d8000.mmc: card claims to support voltages below defined range
[ 2.009895] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 2.016212] mmc1: new SDIO card at address 0001
[ 2.045428] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 2.051570] davinci_mdio 4a101000.mdio: detected phy mask fffffffc
[ 2.059280] libphy: 4a101000.mdio: probed
[ 2.063324] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Atheros 8031 ethernet
[ 2.072637] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Atheros 8031 ethernet
[ 2.082862] cpsw 4a100000.ethernet: Detected MACID = 00:18:31:e7:9f:ed
[ 2.090832] cpsw 4a100000.ethernet: cpsw: Detected MACID = 00:18:31:e7:9f:ee
[ 2.100444] input: gpio_buttons@0 as /devices/gpio_buttons@0/input/input1
[ 2.108158] omap_rtc 44e3e000.rtc: setting system clock to 2012-07-27 12:05:11 UTC (1343390711)
[ 2.120246] ALSA device list:
[ 2.123252] No soundcards found.
[ 2.130080] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[ 2.137511] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[ 2.356736] EXT4-fs (mmcblk0p2): recovery complete
[ 2.364058] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.372370] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[ 2.383054] devtmpfs: mounted
[ 2.386896] Freeing unused kernel memory: 260K (c07d6000 - c0817000)
INIT: version 2.86 booting
Please wait: booting...
Starting udev
[ 3.554933] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 3.727479] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 3.856633] lis3lv02d: 16 bits lis331dlh sensor found
[ 4.025792] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input2
[ 4.237272] davinci_evm sound: tlv320aic3x-hifi <-> 4803c000.mcasp mapping ok
[ 4.769880] musb-hdrc musb-hdrc.0.auto: MUSB HDRC host driver
[ 4.841426] musb-hdrc musb-hdrc.0.auto: new USB bus registered, assigned bus number 1
[ 4.854693] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.861625] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.868906] usb usb1: Product: MUSB HDRC host driver
[ 4.873907] usb usb1: Manufacturer: Linux 3.14.43-g875c69b musb-hcd
[ 4.880216] usb usb1: SerialNumber: musb-hdrc.0.auto
[ 4.887323] hub 1-0:1.0: USB hub found
[ 4.891174] hub 1-0:1.0: 1 port detected
[ 4.900763] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 4.907277] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 4.915424] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.922248] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.929531] usb usb2: Product: MUSB HDRC host driver
[ 4.934519] usb usb2: Manufacturer: Linux 3.14.43-g875c69b musb-hcd
[ 4.940834] usb usb2: SerialNumber: musb-hdrc.1.auto
[ 4.947815] hub 2-0:1.0: USB hub found
[ 4.951635] hub 2-0:1.0: 1 port detected
[ 5.066593] alignment: ignoring faults is unsafe on this CPU. Defaulting to fixup mode.
Remounting root file system...
[ 5.130899] EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
[ 5.141551] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Caching udev devnodes
logger: mount: mount point /proc/bus/usb does not exist
ALSA: Restoring mixer settings...
No state is present for card AM335xEVMSK
Configuring network interfaces... Found hardware: "AM335x-EVMSK" "" "" "" ""
Hardware is initialized using a generic method
No state is present for card AM335xEVMSK
[ 6.880702] net eth0: initializing cpsw version 1.12 (0)
[ 6.966079] net eth0: phy found : id is : 0x4dd074
eth0 no wireless extensions.
udhcpc (v1.13.2) started
Sending discover...
[ 8.749293] random: nonblocking pool is initialized
[ 9.966097] libphy: 4a101000.mdio:00 - Link is Up - 100/Full
Sending discover...
Sending discover...
No lease, forking to background
done.
Setting up IP spoofing protection: rp_filter.
INIT: Entering runlevel: 5
Starting system message bus: dbus.
Starting Hardware abstraction layer hald
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting network benchmark server: netserver.
Starting syslogd/klogd: done
Starting thttpd.
[ 18.424131] Unhandled fault: external abort on non-linefetch (0x1018) at 0xb6ff344c
Bus error
No SGX hardware, not starting PVR
Starting Lighttpd Web Server: lighttpd.
2012-07-27 12:05:27: (log.c.166) server started
[ 18.679202] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 18.953668] kjournald starting. Commit interval 5 seconds
[ 18.961893] EXT3-fs (mmcblk0p3): using internal journal
[ 18.967477] EXT3-fs (mmcblk0p3): recovery complete
[ 18.972313] EXT3-fs (mmcblk0p3): mounted filesystem with ordered data mode
/
Starting Matrix GUI application.
[ 19.528866] Number of LUNs=8
[ 19.531908] Mass Storage Function, version: 2009/09/11
[ 19.539103] LUN: removable file: (no medium)
[ 19.543898] Number of LUNs=2
[ 19.547869] LUN: file: /dev/mmcblk0p1
[ 19.552454] LUN: file: /dev/mmcblk0p3
[ 19.556277] Number of LUNs=2
[ 19.561392] g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
[ 19.568527] g_mass_storage gadget: userspace failed to provide iSerialNumber
[ 19.575684] g_mass_storage gadget: g_mass_storage ready
[ 19.584675] musb-hdrc musb-hdrc.0.auto: otg: usb_otg_register_gadget: device not registered to otg core
[ 19.916399] g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
binutils-symlinks
binutils
gdbserver
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ 62.085784] remoteproc0: failed to load am335x-pm-firmware.elf
[ 62.091837] remoteproc0: powering up wkup_m3
[ 62.102178] remoteproc0: Direct firmware load failed with error -2
[ 62.108649] remoteproc0: Falling back to user helper
[ 62.139045] remoteproc0: request_firmware failed: -2
[ 62.144230] wkup_m3 44d00000.wkup_m3: rproc_boot failed
INIT: Id "S" respawning too fast: disabled for 5 minutes
1.请大家帮忙看看 是哪的问题 就是 进不了输入界面,是 EXT3 EXT4 不兼容的问题吗,还是什么问题 ,刚开始学习,很多不知道,希望大家帮助帮助。
2.ti-processor-sdk-linux-335x-evm-01.00.00.03/filesystem/tisdk-rootfs-image-am335x-evm.tar.gz 这个文件系统怎么用啊 我在官网资料上也没找到制作过程,望大家给点帮助 谢谢了!!