This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教DM368电源问题

Other Parts Discussed in Thread: TPS65001

我用TPS65001给DM368供电,输入5V,输出给DM368三路电源,电压分别为1.35V、1.8V、3.3V,当5V电压上升较慢时(3.3V上电时5V还没上升到3.3V,导致3.3V随着5V一起升高),DM368的1.8V会被拉高到2.3V,目前已经定位到VDDS18引脚,在上电的情况下将该引脚与1.8V电源断开,1.8V电源电压变为正常,而VDDS18引脚的电压为2.6V。 当5V上升较快时,上电的情况下将VDDS18引脚与1.8V断开,测到VDDS18有1.0V的电压。

请问:

1.VDDS18引脚不加电的时候有1.0V电压是不是正常的?

2.如果DM368除了DDR接口之外不使用其他的1.8V IO口,VDDS18能不能悬空,不接电源? 谢谢!

  • Zhijun Zhang2 说:

    1.VDDS18引脚不加电的时候有1.0V电压是不是正常的?

    2.如果DM368除了DDR接口之外不使用其他的1.8V IO口,VDDS18能不能悬空,不接电源? 谢谢!

    1.没有关注过没有上电时候的电源脚电压。请问你测量到的上电时序是否满足芯片的需求?

    2. 除非数据手册里有说明,即使没有使用1.8V的IO,相关电源仍然是要上电的。

  • 1.上电时序满足要求,是按照1.35、1.8、3.3的顺序上的,不过就是在5V上升较慢的时候,3.3V启动时5V还没有达到3.3V,所以3.3V有一个随着5V启动的斜坡,不是陡峭的上升沿。请问这种上升沿不陡峭的3.3V有什么影响?

    2.请问VDDS18是不是给除了DDR之外的1.8V IO 口供电?

  • 你好,

    1. 如果仅仅是3.3V上升比较慢,保证在3.3V稳定前reset信号一直为低是没有什么问题。但你的问题是1.8V超出了spec,这是不允许的。

    2. 还有Internal RAM。

    VDDS18  Power supply for 1.8-V I/O.

    VDD18_SLDO Power supply for internal RAM
    For proper device operation, this pin must be connected to VDDS18.