本人想通过C6678的核0持续的通过网口接受来自ARM端的数据,每次接受一段数据后通知核1,将数据拷贝到核1进行处理,然后核1处理完后,通知核0,再由核0通过网口传回ARM。目前用的是基于sys/bios的UDP例程和IPC,单独的UDP例程、IPC例程均已经调通,但是现在准备将IPC与UDP例程进行融合出现了调用IPC_start函数时(正常情况是核1进入IPC_start函数中,而后当核0达到IPC_start时使得核1从IPC_start函数中出来),核0、核1都进入IPC_start函数中出不来。但是把UDP例程和其配置去除,核0能正常触发核1。请教各位大神,是不是UDP例程有一些配置干扰了IPC的配置导致IPC不能正常触发呢还是其他原因呢?谢谢各位!(说明:使用的是C6678EVM,软件CCS5.2,BIOS版本:6.35.4,NDK版本:2.24.2.31,IPC版本:1.24.3.32;对于IPC与UDP配置文件:将UDP例程中.cfg文件内容拷贝到IPC的.cfg文件中)