Part Number: TMS320C6713B
你好!
我的电脑是win11,软件使用CCS8.3.1,仿真器使用SEED-XDS510PLUS,控制芯片为TMS320C6713B。使用XDS510的仿真器链接控制器,一直报下面的错误。请教下是哪里的问题啊
[Start: SEED XDS510PLUS Emulator_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\yiyue\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'seedjca8990isa.dll'.
The library build date was 'Apr 30 2019'.
The library build time was '14:17:18'.
The library package version is '8.1.0.00012'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '0' (0x00000000).
The controller has an insertion length of '0' (0x00000000).
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-200' (0xffffff38).
The title is 'SC_ERR_TBC_VERSION'.
The explanation is:
The version number of the controller is not valid.
[End: SEED XDS510PLUS Emulator_0]