This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x u-boot DDR3参数如何确定?



u-boot调试方法:设置CPU引脚为串口启动,然后通过超级终端,发送u-boot-spl.bin,u-boot-spl.bin执行到s_init()中的sdram_init后,串口界面就没有C字符输出了,初步怀疑为SDRAM初始化参数错误,请问各位大神,这个判断对吗?另外DDR3参数如何确定呢?内存用的是micron的MT41K512M8


以下是DDR相关参数定义:

#define MT41K512M8RG_EMIF_READ_LATENCY     0x7
#define MT41K512M8RG_EMIF_TIM1                           0x888a39b
#define MT41K512M8RG_EMIF_TIM2                           0x2a517fda
#define MT41K512M8RG_EMIF_TIM3                           0x501f84ef
#define MT41K512M8RG_EMIF_SDREF                      0x0000093B
#define MT41K512M8RG_EMIF_SDCFG                      0x4C000008
#define MT41K512M8RG_RD_DQS                              0x40
#define MT41K512M8RG_WR_DQS                             0x9
#define MT41K512M8RG_PHY_FIFO_WE                  0x7F
#define MT41K512M8RG_PHY_WR_DATA                0xC1
#define MT41K512M8RG_IOCTRL_VALUE                0x18B
#define MT41K512M8RG_ZQ_CFG                             0x50074BE4
#define MT41K512M8RG_RATIO                                0x80
#define MT41K512M8RG_INVERT_CLKOUT          0x0