Part Number: TDA4VEN-Q1
您好,我用SDK编译完成后制作SD启动,在板端执行我这边的模型文件,包括前处理和模型运行,前处理在C7x_2中运行,运行时间不到9毫秒,模型在C7x_1中运行,运行时间135秒.
和您沟通后,运行内部测试程序TI_DEVICE_armv8_test_dl_algo_host_rt.out,从ti-processor-sdk-rtos-j722s-evm-10_00_00_05/c7x-mma-tidl/arm-tidl/rt/out/J722S/A53/LINUX/release中拷贝出来的.
从SDK8.2中中拷贝的运行相关配置文件,从SDK8.2中中拷贝的运行相关配置文件,修改/opt/tidl_test/testvecs/multinet/tidl_infer_multinet.txt,
root@j722s-evm:/opt/tidl_test/testvecs/multinet# cat tidl_infer_multinet.txt
inFileFormat = 2
postProcType = 2
numFrames = 1
#padInBuffInTB = 1
#out-det-quantize
#netBinFile = "testvecs/config/tidl_models/onnx/multinet/test/20220126_bisenet/tidl_net_.bin"
#ioConfigFile = "testvecs/config/tidl_models/onnx/multinet/test/20220126_bisenet/tidl_io_1.bin"
#netBinFile = "testvecs/multinet/model/yolov5_yolox_exp12_epoch75_seg_20220813/tidl_net_.bin"
#ioConfigFile = "testvecs/multinet/model/yolov5_yolox_exp12_epoch75_seg_20220813/tidl_io_1.bin"
#netBinFile = "testvecs/multinet/model/yolov5_yolox_exp12_epoch75_seg_20220813/tidl_net_park.bin"
#ioConfigFile = "testvecs/multinet/model/yolov5_yolox_exp12_epoch75_seg_20220813/tidl_io_park.bin"
netBinFile = "/opt/vision_apps/model//tidl_net_park.bin"
ioConfigFile = "/opt/vision_apps/model//tidl_io_park.bin"
inData = testvecs/multinet/input/file_list_image_bmp.txt
outData = testvecs/multinet/output/out.bin
#debugTraceLevel = 3
#writeTraceLevel = 3
#writeBinAsHeader = 0
#quantRangeUpdateFactor = 0.1
#flowCtrl = 0
postProcDataId = 1
上电运行程序,第一次异常结果
root@j722s-evm:/opt/tidl_test# ./TI_DEVICE_armv8_test_dl_algo_host_rt.out
Processing config file #0 : testvecs/multinet/tidl_infer_multinet.txt
APP: Init ... !!!
13622.845071 s: MEM: Init ... !!!
13622.845169 s: MEM: Initialized DMA HEAP (fd=7) !!!
13622.845415 s: MEM: Init ... Done !!!
13622.845440 s: IPC: Init ... !!!
13622.902301 s: IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
13622.910651 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
13622.915958 s: VX_ZONE_INIT:Enabled
13622.916022 s: VX_ZONE_ERROR:Enabled
13622.916031 s: VX_ZONE_WARNING:Enabled
13622.917745 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-0
13622.918010 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-1
13622.918164 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-2
13622.918285 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:124] Added target MPU-3
13622.918304 s: VX_ZONE_INIT:[tivxInitLocal:136] Initialization Done !!!
13622.918454 s: VX_ZONE_INIT:[tivxHostInitLocal:106] Initialization Done for HOST !!!
13622.966474 s: VX_ZONE_ERROR:[ownContextSendCmd:885] Command ack message returned failure cmd_status: -1
13622.966712 s: VX_ZONE_ERROR:[ownNodeKernelInit:592] Target kernel, TIVX_CMD_NODE_CREATE failed for node TIDLNode
13622.966736 s: VX_ZONE_ERROR:[ownNodeKernelInit:593] Please be sure the target callbacks have been registered for this core
13622.966749 s: VX_ZONE_ERROR:[ownNodeKernelInit:594] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
13622.966767 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:620] kernel init for node 0, kernel com.ti.tidl:1:2 ... failed !!!
13622.966798 s: VX_ZONE_ERROR:[vxVerifyGraph:2254] Node kernel init failed
13622.966811 s: VX_ZONE_ERROR:[vxVerifyGraph:2311] Graph verify failed
TIDL_RT_OVX: ERROR: Verifying TIDL graph ... Failed !!!
TIDL_RT_OVX: ERROR: Verify OpenVX graph failed
# NETWORK_INIT_TIME = 134.17 (in ms, c7x @1GHz)
----------------------- TIDL Process with TARGET DATA FLOW ------------------------
13623.056164 s: VX_ZONE_ERROR:[ownContextSendCmd:885] Command ack message returned failure cmd_status: -1
13623.056211 s: VX_ZONE_ERROR:[ownNodeKernelInit:592] Target kernel, TIVX_CMD_NODE_CREATE failed for node TIDLNode
13623.056224 s: VX_ZONE_ERROR:[ownNodeKernelInit:593] Please be sure the target callbacks have been registered for this core
13623.056237 s: VX_ZONE_ERROR:[ownNodeKernelInit:594] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
13623.056255 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:620] kernel init for node 0, kernel com.ti.tidl:1:2 ... failed !!!
13623.056276 s: VX_ZONE_ERROR:[vxVerifyGraph:2254] Node kernel init failed
13623.056288 s: VX_ZONE_ERROR:[vxVerifyGraph:2311] Graph verify failed
13623.056518 s: VX_ZONE_ERROR:[ownGraphScheduleGraphWrapper:919] graph is not in a state required to be scheduled
13623.056532 s: VX_ZONE_ERROR:[vxProcessGraph:844] schedule graph failed
13623.056543 s: VX_ZONE_ERROR:[vxProcessGraph:849] wait graph failed
ERROR: Running TIDL graph ... Failed !!!
# NETWORK_EXECUTION_TIME = 18.04 (in ms, c7x @1GHz) with DDR_BANDWIDTH (Read + Write) = 0.00, 0.00, 0.00 (in Mega Bytes/frame)Error at line: 756 : in file /home/liguangying/work/TIVEN/ti-processor-sdk-rtos-j722s-evm-10_00_00_05/c7x-mma-tidl/arm-tidl/rt/test/armv8/../src/tidl_tb.c, of function : tidlMultiInstanceTest
Invalid Error Type!
Error at line: 762 : in file /home/liguangying/work/TIVEN/ti-processor-sdk-rtos-j722s-evm-10_00_00_05/c7x-mma-tidl/arm-tidl/rt/test/armv8/../src/tidl_tb.c, of function : tidlMultiInstanceTest
Invalid Error Type!