This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Do you guys know the difference between intel core 7 and intel core i7



What is the difference between intel core 7 and intel core i7?

It seems like you’re asking about the difference between Intel Core 7 and Intel Core i7, but there's a bit of confusion here.

  1. Intel Core i7: This is a specific model line within Intel’s Core processor family. The i7 series is known for offering high performance, generally used in mid- to high-end desktop computers, laptops, and workstations. These processors are usually more powerful than the i3 and i5 models and are intended for demanding tasks like gaming, video editing, and multitasking.

  2. Intel Core 7: This term is not a recognized processor family or specific model. You might be referring to the Intel Core i7 series, but if you’ve seen it written as "Intel Core 7," it could be a typo or an incomplete reference to the i7.

To summarize, Intel Core i7 is the correct and full name for the series of processors. "Intel Core 7" doesn’t refer to a specific product.

i just write this article, i dont know if it is ok: www.sinsmarts.com/.../