你好,问下C6713B的PLLCSR寄存器中有POWERDWN控制位,PLL初始化时是否支持PLLCSR = 0x02来关断PLL,还是必须用PLLCSR = 0x08复位PLL
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,问下C6713B的PLLCSR寄存器中有POWERDWN控制位,PLL初始化时是否支持PLLCSR = 0x02来关断PLL,还是必须用PLLCSR = 0x08复位PLL
谢谢!
你好,最近我用了SM32C6713BGDPM30EP芯片共计8片,其中发现有3片在低温-40度环境下DSP运行异常
最终排查发现此DSP在低温-40度环境下初始化时若采用PLLCSR = 0x08(复位)启动DSP,则会出现DSP读取FLASH数据异常的错误
若在低温-40度环境下初始化时采用PLLCSR = 0x02(断电)启动DSP,则DSP运行正常,故障不再出现
经过反复更换两种代码,采用PLL复位模式启动总是有问题,用PLL断电模式启动总是正常
问下:对于30EP这款芯片是否必须采用PLLCSR = 0x02(断电)才可在低温环境下正常工作?
再问下:对于PLLCSR = 0x02(断电)和PLLCSR = 0x08(复位)启动DSP对于DSP有什么影响?
PS:原来我一直用TMS320C6713BGDP-A200芯片,采用低温-40度环境下采用PLLCSR = 0x08(复位)启动DSP一直 没问题,此次也是按照手册采用了PLLCSR = 0x08(复位)的方式在低温时出现故障。