This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6446 DSP SERVER例程跑不通

dm6446的关于dsp server例程lab12a跑不通.(lab11能正常运行)貌似是版本不兼容的问题?警告为:ti.targets.C64P: warning: exec of '/home/user/dvevm_1_10/cg6x_6_0_3/bin/cl6x -version' failed:java.io.IOException: java.io.IOException: /home/user/dvevm_1_10/cg6x_6_0_3/bin/cl6x: cannot execute.interfaces files complete: Sat Jun 9 22:18:18 CST 2012.

报错为:js:  "/home/user/dvevm_1_10/xdctools_1_21/packages/xdc/cfg/cfg.js", line 143: exception from uncaught JavaScript throw: Error: incompatible use of the target 'ti.targets.C64P', imported version [], ti.targets.rts6000 was built using version [1,0,5.2,0,4], ti.sdo.ce.trace was built using version [1,0,6.0,3], ti.sdo.ce.osal.alg was built using version [1,0,6.0,3], ti.bios.utils was built using version [1,0,6.0,3], ti.bios was built using version [1,0,6.0,3], ti.rtdx was built using version [1,0,6.0,3], ti.sdo.ce.osal was built using version [1,0,6.0,3], ti.sdo.fc.dskt2 was built using version [1,0,6.0,3], ti.sdo.fc.dman3 was built using version [1,0,6.0,3], ti.sdo.fc.acpy3 was built using version [1,0,6.0,3], ti.sdo.ce.node was built using version [1,0,6.0,3], ti.sdo.ce was built using version [1,0,6.0,3], ti.sdo.ce.video was built using version [1,0,6.0,3], codecs.videnc_copy was built using version [1,0,6.0,3], codecs.viddec_copy was built using version [1,0,6.0,3], ti.sdo.ce.audio was built using version [1,0,6.0,3], codecs.audenc_copy was built using version [1,0,6.0,3], codecs.auddec_copy was built using version [1,0,6.0,3]

截图: