This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有个问题,Keystone 2的ARM好像没有显示器接口,例如HDMI这类的,也没法接入鼠标键盘之类的,可移植的操作系统貌似也没有图形化界面的,这样的话,ARM在系统中的定位是什么?
我一直以为Keystone 2的ARM能和Xilinx Zynq中的ARM一样,能跑图形化界面Linux,然后接入显示器、鼠标、键盘,这样可以替代主机(例如原来系统中需要一t进行显台PC机进行显示、控制等)
Keystone 2的定位就是用DSP实现通信中的Layer1,ARM实现Layer2、Layer3?
还有别的应用吗?比如成像系统,如果ARM能跑图形化操作系统,是不是更方便?
需要图像输出可以考虑现在的AM5728
http://www.ti.com/product/AM5728
@Allen Yin 求教,
AM5728能支持输入多少路1080p?每次能实现多少路1080p的编码?
66AK2H14没有图像输出接口;ARM上的Linux系统已经完善了,包含在Processor SDK里面。
AM5728内部是2*A15 + 2*C66x的结构,如果DSP能力不够,可以考虑外接C6678,不一定需要K2H14。
如果ARM上仅仅是做显示输出,可以考虑使用AM335x做人机界面;大量数据处理还是要在K2或者K1的DSP上做。
Hi, Allen
AM5728能支持输入多少路1080p?每次能实现多少路1080p的编码?
考虑AM5728用作3路以上高清视频的处理,如压缩、存储等。
ARM A15主要做协议和系统,DSP主要用来做数据处理;具体系统怎么设计取决于你的应用场景,无法一概而论,如果你仅需要做显示和大规模的数据计算,那么我觉得AM335x+C6678更适合你。