This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于6678client例子修改的问题~~!



mcsdk_2_00_08_20版本的client.pjt运行后结果如下,正常了。 进一步请教:我研究NDK starting guide里面将基于6455的client例子经过修改后,达到了6455向PC发送数据的效果,这个我在6455上试验了,可以。请问对6678的client例子做相应的修改可以吗?达到能够单核向PC发送数据

谢谢~!

[C66xx_0] QMSS successfully initialized

[C66xx_0] CPPI successfully initialized

[C66xx_0] PA successfully initialized

[C66xx_0]

[C66xx_0] TCP/IP Stack Example Client

[C66xx_0] Configuring DHCP client

[C66xx_0] PASS successfully initialized

[C66xx_0] Ethernet subsystem successfully initialized

[C66xx_0] Ethernet eventId : 48 and vectId (Interrupt) : 7

[C66xx_0] Registration of the EMAC Successful, waiting for link up ..

[C66xx_0] Service Status: DHCPC    : Enabled  :          : 000

[C66xx_0] Service Status: Telnet   : Enabled  :          : 000

[C66xx_0] Service Status: HTTP     : Enabled  :          : 000

[C66xx_0] Service Status: DHCPC    : Enabled  : Running  : 000

[C66xx_0] Network Added: If-1:192.168.0.194

[C66xx_0] Service Status: DHCPC    : Enabled  : Running  : 017