This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x USB启动问题



我使用ti-processor-sdk-linux-am335x-evm-01.00.00.03-Linux-x86-Install.bin在Ubutu 14.04上安装过后的sdk,在HOST的/opt/ti-processor-sdk-linux-am335x-evm-01.00.00.03/bin/目录中,使用create-sdcard.sh脚本分别创建SD启动卡和USB启动盘(使用pre build的MLO和u-boot.img及内核)。使用SD卡可以启动开发板,加载内核,进入GUI界面。使用U盘无法启动开发板,LCD屏幕都没有亮。在HOST上查看查看SD卡USB设备信息,分区及文件系统等都是一样。请问各位大神,此问题可能是什么原因。

另外am3358-sk开发板上启动顺序最后一个是USB,按照逻辑,前面3个设备都没有u-boot和内核,只能从第四个设备(USB)启动。