This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

gpmc+st16c554d扩展串口没有产生中断的问题



hi:

我现在调试gpmc+st16c554d扩展串口,遇到的问题是:gpmc读写st16c554d的寄存器都是正常的(通过读取st16c554d的相关寄存器初始值,写数据到st16c554d寄存器,然后读取来验证gpmc的正确性),配置st16c554d如下:

   //config baud rate 115200

    writeb(0x80, fifo_base_addr+lcr);
    writeb(0x01, fifo_base_addr+dll);
    writeb(0x0, fifo_base_addr+dlm);


    //lcr----data bit is 8,no parity,stop bit is 1
    writeb(0x03, fifo_base_addr+lcr);
   

    //ier---enable rx interrupt
    writeb(0x01, fifo_base_addr+ier);
   
    //mcr ---Forces the INT (A-D) outputs to the activemode during the 16 mode,0x08
    writeb(0x08, fifo_base_addr+mcr);

现在遇到的问题是:

pc 机通过串口收发工具发送数据到st16c554d芯片上,st16c554d芯片的接收引脚rx能够量出pc发送的数据,但是st16c554d 中断引脚就是不能产生中断,请专家帮我分析一下什么原因,谢谢!