This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2H通过TFTP获取GPH文件错误



请教个问题,如下,

EVMK2H、PC、路由器互联,PC端设置为DHCP。EVMK2H ARM SPI Boot上电后,EVMK2H的IP是192.168.1.100,PC的IP是192.168.1.113。

PC端的TFTP配置为,“tftpd64.exe”软件的根目录下放了1.gph文件,TFTP配置如下图

拟根据EVMK2H光盘中MCSDK安装后的MCSDK 3.X User Guide的第40页进行如下图操作,即EVMK2H通过TFTP Server获取SPI GPH文件。

EVMK2H的UBoot打印如下,

TCI6638 EVM # dhcp 0xc300000 1.gph
BOOTP broadcast 1
*** Unhandled DHCP Option in OFFER/ACK: 52
*** Unhandled DHCP Option in OFFER/ACK: 52
DHCP client bound to address 192.168.1.100
Using TCI6638_EMAC device
TFTP from server 192.168.1.113; our IP address is 192.168.1.100
Filename '.
Load address: 0xc300000
Loading: *
TFTP error: 'File not found' (1)
Not retrying...
TCI6638 EVM #

之前是输入了命令

setenv serverip 192.168.1.113
saveenv

然后在UBoot控制台中输入如下命令

dhcp 0xc300000 1.gph

UBoot控制台打印TFTP File Not Found的错误如下,

TCI6638 EVM # dhcp 0xc300000 1.gph
BOOTP broadcast 1
*** Unhandled DHCP Option in OFFER/ACK: 52
*** Unhandled DHCP Option in OFFER/ACK: 52
DHCP client bound to address 192.168.1.100
Using TCI6638_EMAC device
TFTP from server 192.168.1.113; our IP address is 192.168.1.100
Filename '.
Load address: 0xc300000
Loading: *
TFTP error: 'File not found' (1)
Not retrying...
TCI6638 EVM #

在PC端通过Wireshark抓取EVMK2H和TFTP Server(即PC)之间的通信包如下

我的问题是:

我在EVMK2H端输入dhcp 0xc300000 1.gph,应该EVMK2H会将文件名1.gph通过TFTP协议发送到TFTP Server端,可是Wireshark抓取的不是这样的。这是为什么?而且无论我在EVMK2H端输入什么样的文件名,Wireshark抓取的都是File:\337。

BMC打印见附件1.txt