您好!自己做的C6748单核板,通过Nand Flash启动,常温时(15~20℃测试)正常启动,电路 5V输入电源工作电流约200mA;低温时,约-20℃时发现就一直无法启动,这时5V输入电源工作电流约400mA。检测上电顺序1.3V(CVDD)》1.2V》1.8V》3.3V按顺序上电,两两间延时约400us;RESET复位芯片采用MAX706,有效复位时间为200ms,时序测试正常。
其中,使用的C6748芯片手册描述可满足-40℃工作温度,其他器件选型也满足温度要求。后发现,实际在5℃附近时,便无法启动,工作电流约400mA;这时将RFESET引脚接地碰一下,工作电流改为约70mA,程序仍未启动;进一步再将RESET引脚接地碰一下,程序可启动运行,请问这可能是什么原因造成的?
另外发现,无法启动时,分两种情况,(1)工作电流为400mA时,晶振未起振,此时用示波器探头接触晶振引脚,晶振起振;(2)工作电流为70mA时,晶振起振,频率正确(24MHz)。