Other Parts Discussed in Thread: SYSBIOS
C6678有时候程序运行不稳定,经常会出现
ti.sysbios.gates.GateMutex: line 97: assertion failure: A_badContext: bad calling context. See GateMutex API doc for details.
xdc.runtime.Error.raise: terminating execution
请问这个是不是内存运行不稳定或者是因为DDR3没有初始化;查看了关于ti.sysbios.gates.GateMutex API,没怎么看懂。请教一下各位!
这个我该工程的.cfg文件:
var Memory = xdc.useModule('xdc.runtime.Memory');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
/*BIOS.heapSize = 0x2000;*/
var Task = xdc.useModule('ti.sysbios.knl.Task');
var HeapBuf = xdc.useModule('ti.sysbios.heaps.HeapBuf');
var Log = xdc.useModule('xdc.runtime.Log');
/*
** Allow storing of task names. By default if you name a task with a friendly display name it will not be saved
** to conserve RAM. This must be set to true to allow it. We use friendly names on the Task List display.
*/
//Defaults.common$.namedInstance = true;
Task.common$.namedInstance = true;
var Clock = xdc.useModule ('ti.sysbios.knl.Clock');
/*
** Interface with IPC. Depending on the version of BIOS you are using the
** module name may have changed.
*/
/* Use this for pre BIOS 6.30 */
/* var Sem = xdc.useModule ('ti.sysbios.ipc.Semaphore'); */
/* Use this for BIOS 6.30 plus to get the IPC module */
var Sem = xdc.useModule ('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule ('ti.sysbios.hal.Hwi');
var Ecm = xdc.useModule ('ti.sysbios.family.c64p.EventCombiner');
/*
** Configure this to turn on the CPU Load Module for BIOS.
**
*/
/*
var Load = xdc.useModule('ti.sysbios.utils.Load');
Load.common$.diags_USER4 = Diags.ALWAYS_ON;
*/
var Diags = xdc.useModule('xdc.runtime.Diags');
/* Load the CSL package */
var Csl = xdc.useModule('ti.csl.Settings');
/* Load the CPPI package */
var Cppi = xdc.loadPackage('ti.drv.cppi');
/* Load the QMSS package */
var Qmss = xdc.loadPackage('ti.drv.qmss');
/* Load the PA package */
var Pa = xdc.useModule('ti.drv.pa.Settings');
/* Load the Platform/NDK Transport packages */
var PlatformLib = xdc.loadPackage('ti.platform.evmc6678l');
var NdkTransport = xdc.loadPackage('ti.transport.ndk');
/*
** Sets up the exception log so you can read it with ROV in CCS
*/
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Exc = xdc.useModule('ti.sysbios.family.c64p.Exception');
Exc.common$.logger = LoggerBuf.create();
Exc.enablePrint = true; /* prints exception details to the CCS console */
/*
** Give the Load module it's own LoggerBuf to make sure the
** events are not overwritten.
*/
/* var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.exitFlush = true;
loggerBufParams.numEntries = 64;
Load.common$.logger = LoggerBuf.create(loggerBufParams);
*/
/*
** Use this load to configure NDK 2.2 and above using RTSC. In previous versions of
** the NDK RTSC configuration was not supported and you should comment this out.
*/
var Global = xdc.useModule('ti.ndk.config.Global');
/*
** This allows the heart beat (poll function) to be created but does not generate the stack threads
**
** Look in the cdoc (help files) to see what CfgAddEntry items can be configured. We tell it NOT
** to create any stack threads (services) as we configure those ourselves in our Main Task
** thread hpdspuaStart.
*/
Global.enableCodeGeneration = false;
/* Define a variable to set the MAR mode for MSMCSRAM as all cacheable */
var Cache = xdc.useModule('ti.sysbios.family.c66.Cache');
//Cache.MAR224_255 = 0x0000000f;
var Startup = xdc.useModule('xdc.runtime.Startup');
var System = xdc.useModule('xdc.runtime.System');
/*
** Create a Heap.
*/
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMem.Params();
/*heapMemParams.size = 0x300000;*/
/*heapMemParams.size = 0x800000 + 0x8000*4 + 0x8000*4;*/
/*heapMemParams.size = 0x8000000;*/
heapMemParams.size = 0x800000 + 0x8000*4 + 0x8000*6;
/*heapMemParams.size = 4;*/
heapMemParams.sectionName = "systemHeap";
Program.global.heap0 = HeapMem.create(heapMemParams);
Memory.defaultHeapInstance = Program.global.heap0;
/* This is the default memory heap. */
var Memory = xdc.useModule('xdc.runtime.Memory');
//Memory.defaultHeapSize = 0x300000;
/*Program.heap = 0x10000;*/
Program.sectMap["sharedL2"] = "DDR3";
Program.sectMap["systemHeap"] = "DDR3";
Program.sectMap[".sysmem"] = "DDR3";
Program.sectMap[".args"] = "DDR3";
Program.sectMap[".cio"] = "DDR3";
Program.sectMap[".far"] = "DDR3";
Program.sectMap[".rodata"] = "DDR3";
Program.sectMap[".neardata"] = "DDR3";
Program.sectMap[".cppi"] = "DDR3";
Program.sectMap[".init_array"] = "DDR3";
Program.sectMap[".qmss"] = "DDR3";
Program.sectMap[".cinit"] = "DDR3";
Program.sectMap[".bss"] = "DDR3";
Program.sectMap[".const"] = "DDR3";
Program.sectMap[".text"] = "DDR3";
Program.sectMap[".code"] = "DDR3";
Program.sectMap[".switch"] = "DDR3";
Program.sectMap[".data"] = "DDR3";
Program.sectMap[".fardata"] = "DDR3";
Program.sectMap[".args"] = "DDR3";
Program.sectMap[".cio"] = "DDR3";
Program.sectMap[".vecs"] = "DDR3";
Program.sectMap["platform_lib"] = "DDR3";
Program.sectMap[".far:taskStackSection"] = "L2SRAM";
Program.sectMap[".stack"] = "L2SRAM";
Program.sectMap[".nimu_eth_ll2"] = "L2SRAM";
Program.sectMap[".resmgr_memregion"] = {loadSegment: "L2SRAM", loadAlign:128}; /* QMSS descriptors region */
Program.sectMap[".resmgr_handles"] = {loadSegment: "L2SRAM", loadAlign:16}; /* CPPI/QMSS/PA Handles */
Program.sectMap[".resmgr_pa"] = {loadSegment: "L2SRAM", loadAlign:8}; /* PA Memory */
Program.sectMap[".far:IMAGEDATA"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_OBJMEM"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_PACKETMEM"] = {loadSegment: "L2SRAM", loadAlign: 128};
/*
** Create my dynamic Heap.
*/
/*var heapMemParams2 = new HeapMem.Params;
heapMemParams2.size = 2048; // heapMem是要多少分多少
heapMemParams2.align = 8;
Program.global.task1Heap = HeapMem.create(heapMemParams2);
IHeap_Handle heap = HeapMem_Handle_upCast(task1Heap);*/
/* Required if using System_printf to output on the console */
SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
/********************************************************************************************************************
* Define hooks and static tasks that will always be running. *
********************************************************************************************************************/
/*
** Register an EVM Init handler with BIOS. This will initialize the hardware. BIOS calls before it starts.
**
** If yuo are debugging with CCS, then this function will execute as CCS loads it if the option in your
** Target Configuraiton file (.ccxml) has the option set to execute all code before Main. That is the
** default.
*/
Startup.lastFxns.$add('&EVM_init');
/*
** Create the stack Thread Task for our application.
*/
var tskNdkStackTest = Task.create("&StackTest");
tskNdkStackTest.stackSize = 0x1400*4;
/*tskNdkStackTest.stackSize = 100*1024;*/
tskNdkStackTest.priority = 0x5;
/*
** Create a Periodic task to handle all NDK polling functions.
** If you are using RTSC configuration with NDK 2.2 and above, this is done by default and
** you do not need to do this.
*/
/*var prdNdkClkParams = new Clock.Params ();
prdNdkClkParams.period = 0x64;
prdNdkClkParams.startFlag = true;
Program.global.clockInst1 = Clock.create("&llTimerTick", 5, prdNdkClkParams);
*/
/*
** If you are using RTSC configuration with NDK 2.2 and above, this is done by default, else
** register hooks so that the stack can track all Task creation
Task.common$.namedInstance = true;
Task.addHookSet ({ registerFxn: '&NDK_hookInit', createFxn: '&NDK_hookCreate', });
/* Enable BIOS Task Scheduler */
BIOS.taskEnabled = true;
/*
* Enable Event Groups here and registering of ISR for specific GEM INTC is done
* using EventCombiner_dispatchPlug() and Hwi_eventMap() APIs
*/
Ecm.eventGroupHwiNum[0] = 7;
Ecm.eventGroupHwiNum[1] = 8;
Ecm.eventGroupHwiNum[2] = 9;
Ecm.eventGroupHwiNum[3] = 10;