SDK Ver: 10_00_00
I modify tests/app_tiovx_linux_decode_display_test.c and try to capture and display my sensor video. The block diagram is as follows.
The main function is as follows
The program ran with an error
16552.514009 s: VX_ZONE_ERROR:[ownContextSendCmd:885] Command ack message returned failure cmd_status: -7
16552.514052 s: VX_ZONE_ERROR:[ownNodeKernelInit:592] Target kernel, TIVX_CMD_NODE_CREATE failed for node node_93
16552.514065 s: VX_ZONE_ERROR:[ownNodeKernelInit:593] Please be sure the target callbacks have been registered for this core
16552.514077 s: VX_ZONE_ERROR:[ownNodeKernelInit:594] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
16552.514092 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:620] kernel init for node 0, kernel com.ti.hwa.vpac_viss ... failed !!!
16552.514125 s: VX_ZONE_ERROR:[vxVerifyGraph:2254] Node kernel init failed
16552.514136 s: VX_ZONE_ERROR:[vxVerifyGraph:2311] Graph verify failed
[TIOVX_MODULES][ERROR] 791: tiovx_modules_verify_graph: Graph Verify failedverify status[-1]
There is no error when I delete the VISS node.I wonder how to solve this porblem.