由于EVM板的BSL没有提供McBSP样例(因为EVM板上的AIC codec是接在McASP口上的),而很多用户有同样的需求。所以写了这么一个简单的McBSP接口的中断例程。
由于EVM板上没有外设与McBSP相连,所以配置为内部产生帧同步,时钟(频率随便配了一个),这仅是一个接口使用的例子,听不到声音的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
由于EVM板的BSL没有提供McBSP样例(因为EVM板上的AIC codec是接在McASP口上的),而很多用户有同样的需求。所以写了这么一个简单的McBSP接口的中断例程。
由于EVM板上没有外设与McBSP相连,所以配置为内部产生帧同步,时钟(频率随便配了一个),这仅是一个接口使用的例子,听不到声音的。
谢谢!
最近在调试 mcbsp_test 驱动的时候,发现word_len为8,frame_len为8或16时都正常,但frame_len如果>=32会出现发送错误,按照“MODULE_PARM_DESC(frame_len, "Frame Length: 1-128 (default:2)");”的说明,frame_len应该可以达到128的,请教下这会什么原因呢,有什么解决方法或思路吗?关于mcbsp驱动编写请做些指导。
源代码如下:
#include <linux/module.h>
#include <linux/init.h>
#include <linux/errno.h>
#include <linux/types.h>
#include <linux/interrupt.h>
#include <linux/io.h>
#include <linux/moduleparam.h>
#include <linux/sysctl.h>
#include <linux/mm.h>
#include <linux/dma-mapping.h>
#include <linux/delay.h>
#include <mach/memory.h>
#include <mach/hardware.h>
#include <mach/irqs.h>
#include <mach/edma.h>
#include <mach/mcbsp.h>
static dma_addr_t physsrc = 0;
static char *bufsrc = NULL;
static dma_addr_t physdest = 0;
static char *bufdest = NULL;
static int device_id = 1;
static int buf_size = (1 * 1024);
static int buf_fmt = 0;
static int num_pkts = 1;
static int word_len = 8;
static int frame_len = 32;
static int freq = 48000;
static bool dlb = 1;
static int numevt = 0;
static int mc_mode = 0;
static int master = 1;
static int tx_rx = 3;
module_param(device_id, int, S_IRUGO);
module_param(buf_size, int, S_IRUGO);
module_param(buf_fmt, int, S_IRUGO);
module_param(num_pkts, int, S_IRUGO);
module_param(word_len, int, S_IRUGO);
module_param(frame_len, int, S_IRUGO);
module_param(freq, int, S_IRUGO);
module_param(dlb, bool, S_IRUGO);
module_param(numevt, int, S_IRUGO);
module_param(mc_mode, int, S_IRUGO);
module_param(master, int, S_IRUGO);
module_param(tx_rx, int, S_IRUGO);
MODULE_PARM_DESC(device_id, "McBSP instance (default:1)");
MODULE_PARM_DESC(buf_size, "Buffer Size (default:1KB)");
MODULE_PARM_DESC(buf_fmt, "Buffer format (default:Interleaved)");
MODULE_PARM_DESC(buf_size, "Packet count (default:1)");
MODULE_PARM_DESC(word_len, "Word Length: 8, 16, 24, 32 bits (default:32)");
MODULE_PARM_DESC(frame_len, "Frame Length: 1-128 (default:2)");
MODULE_PARM_DESC(freq, "Sample Frequency (default:48kHz)");
MODULE_PARM_DESC(dlb, "Digital Loopback (default: disabled)");
MODULE_PARM_DESC(numevt, "NUMEVT (default: 0)");
MODULE_PARM_DESC(mc_mode, "Multi-channel mode (default: 0)");
MODULE_PARM_DESC(master, "Master/Slave mode (default: master)");
MODULE_PARM_DESC(tx_rx, "Transmit, Receive or both (default: both)");
static int __init mcbsp_test_init(void)
{
struct davinci_mcbsp_dev *dev = NULL;
int i;
int loopcnt = 0;
int errcnt;
if (tx_rx & 0x01) {
bufsrc = dma_alloc_coherent(NULL, buf_size, &physsrc, 0);
if (!bufsrc) {
printk ("dma_alloc_coherent failed for physsrc\n");
return -ENOMEM;
}
for (i = 0; i < buf_size; i++)
bufsrc[i] = i % 256;
}
if (tx_rx & 0x02) {
bufdest = dma_alloc_coherent(NULL, buf_size, &physdest, 0);
if (!bufdest) {
printk ("dma_alloc_coherent failed for physdest\n");
return -ENOMEM;
}
}
printk("Starting McBSP test\n");
davinci_mcbsp_request(device_id, &dev);
do {
/* configure rcr and xcr */
dev->tx_params.word_length1 = word_len; /* 32 bits */
dev->tx_params.frame_length1 = frame_len;
dev->rx_params.word_length1 = word_len; /* 32 bits */
dev->rx_params.frame_length1 = frame_len;
dev->rx_params.buf_fmt = buf_fmt;
dev->tx_params.buf_fmt = buf_fmt;
if (mc_mode > 0 && mc_mode < 8) {
dev->rx_params.intr_mode = 1;
dev->tx_params.intr_mode = 1;
}
davinci_mcbsp_config_params(dev, master);
/* sample rate generator conifguration */
davinci_mcbsp_config_clock(dev, freq);
dev->tx_params.numevt = numevt;
dev->rx_params.numevt = numevt;
dev->tx_params.numdma = 1;
dev->rx_params.numdma = 1;
davinci_mcbsp_config_fifo(dev);
dev->tx_params.mc_mode = mc_mode;
dev->rx_params.mc_mode = mc_mode;
dev->tx_params.cer[0] = 0x5555;
dev->tx_params.cer[1] = 0x5555;
dev->tx_params.cer[2] = 0x5555;
dev->tx_params.cer[3] = 0x5555;
dev->tx_params.cer[4] = 0x5555;
dev->tx_params.cer[5] = 0x5555;
dev->tx_params.cer[6] = 0x5555;
dev->tx_params.cer[7] = 0x5555;
dev->rx_params.cer[0] = 0x5555;
dev->rx_params.cer[1] = 0x5555;
dev->rx_params.cer[2] = 0x5555;
dev->rx_params.cer[3] = 0x5555;
dev->rx_params.cer[4] = 0x5555;
dev->rx_params.cer[5] = 0x5555;
dev->rx_params.cer[6] = 0x5555;
dev->rx_params.cer[7] = 0x5555;
davinci_mcbsp_config_multichannel_mode(dev);
/* DMA Mode */
dev->op_mode = DAVINCI_MCBSP_DMA_MODE;
if (dlb) {
printk("Setting DLB mode \n");
dev->op_mode |= DAVINCI_MCBSP_DLB_MODE;
} else {
printk("No DLB mode \n");
}
if (tx_rx & 0x01) {
printk("Transmitting Packet %d\n", loopcnt + 1);
for (i = 0; i < buf_size; i++)
bufsrc[i] = (i + loopcnt) % 256;
printk("Starting McBSP TX\n");
davinci_mcbsp_start_tx(dev);
}
if (tx_rx & 0x02) {
printk("Starting McBSP RX\n");
davinci_mcbsp_start_rx(dev);
}
printk("McBSP started\n");
if (tx_rx & 0x02) {
printk("Receving data...\n");
davinci_mcbsp_recv_buf(dev, physdest, buf_size);
}
if (tx_rx & 0x01) {
printk("Transmitting data...\n");
davinci_mcbsp_xmit_buf(dev, physsrc, buf_size);
}
if (dev->op_mode & DAVINCI_MCBSP_DLB_MODE) {
wait_for_completion(&dev->tx_params.dma_completion);
printk("...TX complete\n");
wait_for_completion(&dev->rx_params.dma_completion);
printk("...RX complete\n");
}
if (tx_rx & 0x01) {
davinci_mcbsp_stop_tx(dev);
printk("TX stopped\n");
}
if (tx_rx & 0x02) {
davinci_mcbsp_stop_rx(dev);
printk("RX stopped\n");
}
if (tx_rx & 0x02 || (dev->op_mode & DAVINCI_MCBSP_DLB_MODE)) {
printk("Testing data integrity for Packet %d: ", loopcnt + 1);
errcnt = 0;
for (i = 0; i < buf_size; i++) {
if (bufdest[i] != ((i + loopcnt) % 256)) {
errcnt = i + 1;
break;
}
}
if (errcnt) {
#if 1 /* debug */
for (i = 0; i < buf_size; i++) {
if (!(i % 10))
printk("\nbufdest[%d]: ", i);
printk("%d\t", bufdest[i]);
}
printk("\n");
#endif
printk("Error found at Byte %d location\n", errcnt);
davinci_mcbsp_dump_reg(dev);
} else
printk("Passed\n");
memset(bufdest, 0 , buf_size);
} else {
mdelay(100);
/* more time to compare data for large buffers */
if (buf_size > 16 * 1024)
mdelay(1000);
if (buf_size >= 32 * 1024)
mdelay(1000);
}
printk("-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.");
printk("-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.-.\n");
} while (++loopcnt < num_pkts);
#if 0 /* debug */
davinci_mcbsp_dump_reg(dev);
#endif
return 0;
}
static void mcbsp_test_exit(void)
{
davinci_mcbsp_free(device_id);
if (tx_rx & 0x01)
dma_free_coherent(NULL, buf_size, bufsrc, physsrc);
if (tx_rx & 0x02)
dma_free_coherent(NULL, buf_size , bufdest, physdest);
printk("McBSP test done... exiting\n");
}
module_init(mcbsp_test_init);
module_exit(mcbsp_test_exit);
MODULE_AUTHOR("Texas Instruments");
MODULE_LICENSE("GPL");