This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

提高OMAPL13x, C674x EMIFA read throughput.



大家反映OMAPL138(C6748)等器件的EMIFA的CPU读写效率比较低,这是由于芯片内部总线架构决定的。如果应用中需要高速的EMIFA读写,建议采用EDMA方式取代CPU读写。

如下图所示,采用EDMA方式,可以实现32byte的连接读写时序。(由于SCR的BR7将大于32byte的访问分成以32byte为单位的访问,所以是最多只能连续32byte的连续访问)。 

在配置EDMA时,如果希望达到最高吞吐率,要将A count设为32byte,或者32byte的倍数。

这里要注意的是:通常EMIFA连接FPGA以FIFO形式访问,地址固定,这种配置下,EMIFA在传输A count个数的数据期间,地址会自动增加,这需要FPGA为该FIFO端口预留出足够的地址空间,以免访问超出该端口的范围。