Other Parts Discussed in Thread: AM3359
我们现在在开发AM3359芯片,使用的Nandflash是三星的K9F1G08,内核可以起来,但是在读文件系统的时候出现以下错误:
omap2-nand driver initializing
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bi t)
Creating 8 MTD partitions on "omap2-nand.0":
0x000000000000-0x000000020000 : "SPL"
0x000000020000-0x000000040000 : "SPL.backup1"
0x000000040000-0x000000060000 : "SPL.backup2"
0x000000060000-0x000000080000 : "SPL.backup3"
0x000000080000-0x000000260000 : "U-Boot"
0x000000260000-0x000000280000 : "U-Boot Env"
0x000000280000-0x000000780000 : "Kernel"
0x000000780000-0x000008000000 : "File System"
write_size=2048,erase_size=131072
OneNAND driver initializing
UBI: attaching mtd7 to ubi0
UBI: physical eraseblock size: 131072 bytes (128 KiB)
UBI: logical eraseblock size: 126976 bytes
UBI: smallest flash I/O unit: 2048
UBI: sub-page size: 512
UBI: VID header offset: 2048 (aligned 2048)
UBI: data offset: 4096
UBI: max. sequence number: 13
UBI warning: print_rsvd_warning: cannot reserve enough PEBs for bad PEB handling , reserved 8, need 9
UBI: attached mtd7 to ubi0
UBI: MTD device name: "File System"
UBI: MTD device size: 120 MiB
UBI: number of good PEBs: 962
UBI: number of bad PEBs: 2
UBI: number of corrupted PEBs: 0
UBI: max. allowed volumes: 128
UBI: wear-leveling threshold: 4096
UBI: number of internal volumes: 1
UBI: number of user volumes: 1
UBI: available PEBs: 0
UBI: total number of reserved PEBs: 962
UBI: number of PEBs reserved for bad PEB handling: 8
UBI: max/mean erase counter: 2/0
UBI: image sequence number: 1473746861
UBI: background thread "ubi_bgt0d" started, PID 513
CAN device driver interface
CAN bus driver for Bosch D_CAN controller 1.0
usbcore: registered new interface driver zd1201
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver dm9601
cdc_ncm: 04-Aug-2011
usbcore: registered new interface driver cdc_ncm
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mousedev: PS/2 mouse device common for all mice
input: ti-tsc-adcc as /devices/platform/omap/tsc/input/input0
i2c /dev entries driver
Linux video capture interface: v2.00
OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
_regulator_get: deviceless supply vdd_mpu not found, using dummy regulator
cpuidle: using governor ladder
cpuidle: using governor menu
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
usbcore: registered new interface driver snd-usb-audio
ALSA device list:
No soundcards found.
oprofile: hardware counters not available
oprofile: using timer interrupt.
nf_conntrack version 0.5.0 (3962 buckets, 15848 max)
ip_tables: (C) 2000-2006 Netfilter Core Team
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Registering the dns_resolver key type
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
ThumbEE CPU extension supported.
mux: Failed to setup hwmod io irq -22
Power Management for AM33XX family
UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PE B 3:4096, read 126976 bytes
UBI error: ubi_io_read: error -74 (ECC error) while reading 126976 bytes from PE B 4:4096, read 126976 bytes