TI的各位专家,你们好
板子用的是EVM6657的板子,按照附件上的步骤一步一步来做的,完了之后,将板子配置成I2C NAND FLASH Image0 启动,然后启动板子,打开串口,串口调试一直打印:IBL:Booting from NAND.我是直接将CCS编译生成的.out文件改成.bin文件烧写到Flash的,确定文件的格式是ELF格式的,也把ibl.bootModes[1].u.nandBoot.bootFormat = ibl_BOOT_FORMAT_BBLOB改成了ibl.bootModes[1].u.nandBoot.bootFormat = ibl_BOOT_FORMAT_ELF。6657的nand的block的大小是131072,nand_writer_input.txt的start_addr也设置的是131072。在Nand Flash中烧写的程序是C:\ti\mcsdk_2_00_09_21\tools\post\evmc6657l\bin\post_evm6657l.out。用同样的步骤,同样的程序,通过I2C NOR Flash启动成功了,可是I2C NAND FLASH启动就一直打印IBL:Booting from NAND.