This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
C54xx: Trouble Reading Memory Block at 0x6 on Page 1 of Length 0x8: Error 0x80000002/-1052 Fatal Error during: Memory, Device driver: Emulator Controller not responding The targets should be power cycled or hard reset followed by an emureset and reconnect to each
target. Then it is recommended to RESET EMULATOR. This will disconnect each target from the emulator.
仿真器XDS100-V2,在学习板上确认过,没有问题CCS4.2
用示波器检查,3.3V和1.8V电源平稳,晶振20M正常;CLKOUT为10M,有轻微过冲(0.4~0.5V),不过跟学习板的波形差不多;复位引脚接MAX809,3.3V。
有一个奇怪的现象,上电后,悬空的INT0~INT3以及NMI为低电平,接上10k电阻上拉后为高,但依然是提示此问题。
请问这个问题可能是什么原因造成的?特别是为什么中断引脚上电后为低电平?学习板上悬空的中断引脚是高的
怎么表格看不见
管脚 电平 管脚 电平 管脚 电平
IACK 低 HD0~HD7, HRDY,HDS1~2 低 MCBSP0,1相关 低
NMI 低 HCNTL0~1,HR/W,HBIL, 低 TOUT0 152.6Hz
INT0~3 低 BIO 低 CLKOUT 10MHz
管脚 所接电平 管脚 所接电平 管脚 所接电平
HPIENA 3.3V READY 3.3V MP/MC 0
HAS 3.3V HOLD 3.3V CLKMD1,2,3 3.3V
这两个管脚拉高了的。
View Memory窗口中,没有一个内存地址是能够读出来的,全部都是问号。
这个仿真器(XDS100-V2)在学习板和另一块自制的DSP板上都用得挺好的(都是5402)。
用示波器测了下新做的这块有问题的核心板的JTAG引脚,下载程序过程中,TMS,TDI,TDO,TRET,TCK(即1,3,7,9,11脚)有波形,TRST,EM0,EM1(2,13,14)一直维持原状,程序下不进去,问题一直是Touble Reading Memory Block。
改天再找个其他型号的仿真器试一下。
供电,晶振,复位,都正常啊,CLKOUT,TOUT0有波形输出,会是什么原因造成无法用仿真器下程序呢?