This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
项目需求Linux+视频处理。我浏览了TI的达芬奇系类初步选择使用DM3725或者TMS320DM8148,但是看到开发模块的价格后我放弃了,因为有点贵最便宜的都要9000人民币。
无意中看到C600的ARM+DSP这个选项,点击进去发现OMAP_L138这款片子和我的要去相符并且开发套件只要200美元。
我仔细对比了一DM3725和OMAP_L138的资源发现相差无几,我想问一下OMAP_L138为什么没有归为达芬奇系列,和达芬奇系列的芯片有何区别?
Davinci 系列的片子侧重于视频处理,你可以看到这个系列一般都具备:
- 比较强的视频接口, 如单路/多路高清视频输入输出接口, 并口/串口 image sensor接口 等
- 视频处理硬件(注意是硬件) 如 ISP, 缩放器, De-interlace module, CSC , 硬件Codec等等
很重要的一点是,上面用的软件也是和应用非常的相关,比如davinci系列上针对安防的IPNCRDK/DVRRDK 等等
拿DM3725和OMAP 138举例,核心的都是ARM+DSP的架构。但是DM的器件多出ISP可以直接接raw data的CCD/CMOSsensor,比138上只能接标清的摄像头要厉害。而且DM37上ARM 1G,DSP 800MHz, 很明显的可以看出和138的差异的。DM37 上还集成了硬件的显卡SGX530,这个也是OMAPL138上不可选的。
一般去选片子,除了看ARM+DSP的架构,ARM/DSP的核心版本,频率之外,还需要看接口、硬件加速器、软件配套等等综合考虑。希望可以帮到你。
你可以提提你的具体需求,我可以给你推荐合适的芯片
您好,感谢您对我的提问做出如此详细的回答。还有一个问题,除了TI官方的DM3725开发套件有没有稍微价格便宜一点的其他公司开发的套件,能与TI给出的软件开发包兼容的。因为9000元一套的开发套件的确是有点贵。