This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm368 dvsdk4.02 如何控制帧率(framerate)1080i 30



我在dm368平台上测试1080i(./encode - y 5 - I 3 ),编码输出信息如下:

ARM Load: 41% Video fps: 27 fps Video bit rate: 4478 kbps Sound bit rate: 0 kbps
 Time: 00:08:16 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 30% Video fps: 28 fps Video bit rate: 4228 kbps Sound bit rate: 0 kbps
 Time: 00:08:17 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 47% Video fps: 20 fps Video bit rate: 4148 kbps Sound bit rate: 0 kbps
 Time: 00:08:18 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 62% Video fps: 19 fps Video bit rate: 4279 kbps Sound bit rate: 0 kbps
 Time: 00:08:19 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 39% Video fps: 27 fps Video bit rate: 4139 kbps Sound bit rate: 0 kbps
 Time: 00:08:20 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 39% Video fps: 26 fps Video bit rate: 4853 kbps Sound bit rate: 0 kbps
 Time: 00:08:20 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

ARM Load: 39% Video fps: 20 fps Video bit rate: 5201 kbps Sound bit rate: 0 kbps
 Time: 00:08:20 Demo: Encode Display: 1080I 30Hz Video Codec: H.264 HP Resolutio
n: 1920x1080 Sound Codec: N/A Sampling Freq: N/A

.....................

从上面输出信息来看,Video fps: 视频编码帧率输出变化幅度较大,不知什么原因,视频丢帧是肯定的,请问如何能控制帧率(framerate),让其 Video fps尽量固定在某值。谢谢........

  • 请问你是在TI DM368 EVM上用原装的软件得到上述结果的么?

    如果不是,看起来是编码能力不够了,你除了编码还做了什么工作?能否把预览显示关闭?

    在DM368 IPNC参考设计上是可以实现1080p30的编码+网传,但是是没有预览的。

    实际的frame rate是每秒调用调用process 的次数。这是应用程实现的。