This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,I want to use Main domain I2c(CSL_I2C2 bitRate 400khz) in Mcu domain. Is it possible to use it in the following way?
1、Set pinmux U23 as I2c SCL, U26 as I2c SDA
2、Preventing access to I2c2 by changing the base address
#define CSL_I2C2_CFG_BASE (0x2020000UL)
#define I2C2_INSTANCE 3
void setConfigI2C(uint8_t instance, uint32_t baseAddr) /* change base address */
{
I2C_HwAttrs i2cCfg;
I2C_socGetInitCfg(instance, &i2cCfg);
i2cCfg.baseAddr = baseAddr;
i2cCfg.enableIntr = 0U;
I2C_socSetInitCfg(instance, &i2cCfg);
}
void test()
{
I2C_Params Commoni2cParams;
I2C_Transaction i2cTransaction;
I2C_Handle i2cHandle = NULL;
I2C_init();
setConfigI2C(I2C2_INSTANCE,CSL_I2C2_CFG_BASE);
I2C_Params_init(&Commoni2cParams);
Commoni2cParams.transferMode = I2C_MODE_BLOCKING;
Commoni2cParams.bitRate = I2C_400kHz;
Commoni2cParams.transferCallbackFxn = NULL;
i2cHandle = I2C_open(I2C2_INSTANCE, &Commoni2cParams);
I2C_transactionInit(&i2cTransaction);
'' set buffer and data size ''
I2C_transfer(i2cHandle, &i2cTransaction);
}
Thanks
Hi
Have you taken a look at the I2C eeprom read example within the RTOS PDK? You can find it at <PDK_PATH>/packages/ti/drv/i2c/test/eeprom_read/src/main_test.c
I believe you have the main steps other than enabling interrupt and selecting the intNum. Ensure to call Board_init() as done in the example to set up pinmux, clocking, and UART stdio.
Hi,I write code based on the sample.
The currently used TDA4 j721E. We used WKUP_I2C0, MCU_I2C0, and Main_I2C2 in Mcu1_0. Using the same code method in mcu1_0, both WKUP_I2C0 and MCU_I2C0 can successfully communicate with external devices. Main_i2C2 and peripheral communication failed.
The following is the code for operating main_i2c2 in mcu1_0. Please help check if there is any problem.
#define CSL_I2C2_CFG_BASE (0x2020000UL)
#define I2C2_INSTANCE 3
#define CSLR_R5FSS0_INTROUTER0_IN_I2C2_POINTRPEND_0 (183U)
I2C_Params Commoni2cParams;
static void setConfigI2C(uint8_t instance, uint32_t baseAddr)
{
I2C_HwAttrs i2cCfg;
I2C_socGetInitCfg(instance, &i2cCfg);
i2cCfg.baseAddr = baseAddr;
i2cCfg.enableIntr = 0U;
if(I2C2_INSTANCE == instance)
{
i2cCfg.intNum = CSLR_R5FSS0_INTROUTER0_IN_I2C2_POINTRPEND_0;
}
I2C_socSetInitCfg(instance, &i2cCfg);
}
void All_I2C_Init_Process()
{
Board_initCfg boardCfg;
boardCfg = BOARD_INIT_PINMUX_CONFIG | BOARD_INIT_MODULE_CLOCK | BOARD_INIT_UART_STDIO | BOARD_INIT_UNLOCK_MMR;
(void)Board_init(boardCfg);
I2C_init();
setConfigI2C(I2C2_INSTANCE,CSL_I2C2_CFG_BASE);
I2C_Params_init(&Commoni2cParams);
Commoni2cParams.transferMode = I2C_MODE_BLOCKING;
Commoni2cParams.bitRate = I2C_400kHz;
Commoni2cParams.transferCallbackFxn = NULL;
}
void I2c_Transmit_Test(uint32_t slaveAddr,uint8_t *writeData, uint32_t numWriteBytes,uint8_t *readData, uint32_t numReadBytes)
{
uint8_t retval = 0;
int8_t status = 0U;
I2C_Transaction i2cTransaction;
I2C_Handle i2cHandle = NULL;
i2cHandle = I2C_open(I2C2_INSTANCE, &Commoni2cParams);
if(NULL == i2cHandle)
{
retval = 1;
}
else
{
I2C_transactionInit(&i2cTransaction);
i2cTransaction.slaveAddress = slaveAddr;
i2cTransaction.writeBuf = (uint8_t *)&writeData[0];
i2cTransaction.writeCount = numWriteBytes;
i2cTransaction.readBuf = (uint8_t *)&readData[0];
i2cTransaction.readCount = numReadBytes;
status = I2C_transfer(i2cHandle, &i2cTransaction);
if(I2C_STS_SUCCESS != status)
{
retval = 2;
}
I2C_close(i2cHandle);
}
The order of function calls is All_I2C_Init_Process(),I2c_Transmit_Test(xx).
when call function I2C_transfer,Discovered function I2C_v1_waitForPin()entering a dead loop. Reg I2C_IRQSTATUS_RAW value is 0.
function I2C_v1_waitForPin():
status = I2CMasterIntRawStatus(hwAttrs->baseAddr);
while ((uint32_t) 0U == (status & flag))
{
}
In summary, please help confirm whether the Main domain I2c can be used in mcu1_0. If can use,please help to investigate the reasons why it is not working well.
Thank you
Hi,
Can you confirm if you would like to configure I2C with interrupts or polling? I see you have selected the correct intNum on the R5 INTRTR, however, you are disabling the enableIntr in the I2C cfg.
Is this a TI EVM or custom board? Can you confirm you have the correct device address and register address you would like to read?
Thanks,
Links