This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,I want to use Uart3 in main domain(baudRate is 460800,use interrupt mode). Is it possible to use it in the following way?
1、Set Pinmux V28 UART3_RXD,V29 UART3_TXD
2、use UART_socSetInitCfg()function set operMode is UART13x_OPER_MODE,set enableInterrupt is TRUE ,baseAddr is (uint32_t)CSL_UART0_BASE + (0x10000U * 3),intNum is CSLR_R5FSS0_INTROUTER0_IN_UART3_USART_IRQ_0。
Sample Code :
UART_init();
UART_socGetInitCfg(3, &uart_cfg);
uart_cfg.edmaHandle = NULL;
uart_cfg.dmaMode = FALSE;
uart_cfg.operMode = UART13x_OPER_MODE;
uart_cfg.loopback = FALSE;
uart_cfg.enableInterrupt = TRUE;
uart_cfg.frequency = UART_INPUT_CLK_48M;
uart_cfg.baseAddr = (uint32_t)CSL_UART0_BASE + (0x10000U * 3);
uart_cfg.intNum = CSLR_R5FSS0_INTROUTER0_IN_UART3_USART_IRQ_0;
UART_socSetInitCfg(uartTestInstance, &uart_cfg);
3、set Params:set baudRate 460800, set writeMode and readMode is UART_MODE_CALLBACK, set writeCallback and readCallback function
Sample Code:
UART_Params_init(&uartParams);
uartParams.baudRate = 460800;
uartParams.writeMode = UART_MODE_CALLBACK;
uartParams.writeCallback = UART_Write_Callback_test;
uartParams.readMode = UART_MODE_CALLBACK;
uartParams.readCallback = UART_Read_Callback_test;
4、use UART_open(3, &uartParams);,then if fifo reach tx/rx Level, write/read callback function is be trigered.
5、Please help answer one more question, Has the Fifo level interrupt been enabled according to the above configuration process. If not, please help provide the activation method. Thank you
zt
Hi,
The UART initialization seems correct, this is non-DMA mode correct? Please look at the UART read/write examples within the SDK for help with setup.
5、Please help answer one more question, Has the Fifo level interrupt been enabled according to the above configuration process. If not, please help provide the activation method. Thank you
I will look into this and get back to you.
Hi,
Please refer to the following patch to enable baud rate of 460800.
Please note this patch is based on SDK 9.2 and you may have to make some minor changes.
Thanks,
https://e2echina.ti.com/cfs-file/__key/communityserver-discussions-components-files/120/uart_5F00_480600_5F00_support.patchPlease check it