本人现在项目需要一款控制3个及以上网口的ARM芯片,在产品栏查询之后觉得AM5K2E04(下面用AM5代替)满足我的需求。而在芯片AM5的页面中,推荐的开发板为K2E开发板,上面使用的处理器芯片是66AK2E05(下面用66A代替)。我对比了一下AM5和66A,发现66A多了个C66x的DSP核,AM5则是一个单纯的ARM芯片,不知道它俩的区别是否是我说的那样?那这样的话66A应该能实现AM5的所有功能是吗?如果我购买了K2E开发板,并插上RTM-Break-out Card,在上面完成了我的项目,只是控制网口的传输,请问之后如果我要画自己的板子的时候能否直接用AM5芯片来替代66A芯片呢?