请问,AISgen for D800K008 在General中若把Boot Mode设置为Nand Flash后为什么Flash选项中就自动变成了CS3 Setup,我现在使用的是C6748,Nand Flash接的片选是CS2,请问我需要怎么使用这个软件把out文件转换成Bin文件呢?是不是规定了C6748只要使用Nand Flash就必须使用CS3片选口呢?我现在硬件接的是CS2口,该怎么办?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问,AISgen for D800K008 在General中若把Boot Mode设置为Nand Flash后为什么Flash选项中就自动变成了CS3 Setup,我现在使用的是C6748,Nand Flash接的片选是CS2,请问我需要怎么使用这个软件把out文件转换成Bin文件呢?是不是规定了C6748只要使用Nand Flash就必须使用CS3片选口呢?我现在硬件接的是CS2口,该怎么办?
nand flash boot mode规定是用CS3片选信号,这在bootloader文档里有说明“NAND Flash should be connected to EMA_CS[3] of the EMIFA peripheral”
http://www.ti.com/lit/an/spraat2f/spraat2f.pdf
您好 能否再帮我解答一个问题,现在我用的是C6748处理器,在里面会用到很多三角函数运算,如cos,sin等,我在文件里面包含了math.h文件了,还有其它头文件需要包含吗?为什么现在出现一个问题是程序运行到cos计算时程序就跑飞了,不知运行到哪里去了。请问如果使用这些三角函数计算需要注意哪些东西呢?