This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教DM8148/8127 关于GPMC_A信号的引脚复用MM(multi-mux )和DVDD_GPMC/DVDD_GPMCB供电问题



项目组准备使用DM8148,本人现在处于DM8148硬件原理图设计阶段。

查看数据手册和参考原理图后,现遇到以下几个问题:

1、我要使用NOR FLASH启动,地址线和数据线不复用,GPMC_A地址线要使用26根,即GPMC_A[26:1],如果GPMC_A[26:1]都选用M0,会有部分信号与视频输入接口VIN1B和EMAC1冲突,想问可以部分地址线选M0,部分地址线选M1吗?比如GPMC_A[15:1]选M1,GPMC_A[26:16]选M0?

——自己在手册上,只找到M0/M1会有时序上的不同,不知道对于GPMC_A有没有必须一组使用的限制。

2、DVDD_GPMC和DVDD_GPMCB供电引脚看手册是可以分开供电的,比如DVDD_GPMC供电3.3V,DVDD_GPMCB供电1.8V(1.8V IO的FLASH),但是BTMODE引脚和GPMC_D复用,手册上Terminal那部分对BTMODE引脚对应DVDD_GPMC,GPMC_D对应DVDD_GPMCB供电,一个担心是一个引脚真的可以适应两种电压吗?另外BOMODE引脚的外部上拉电阻是上拉到3.3V还是1.8V呢?如果是3.3V,会影响GPMC_D的正常使用吗?

3、如果我使用EMAC1,是不是真的不能用EMAC1启动uboot?

希望各大牛不吝赐教,先谢过了!!