This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354,OSC0硬件设计石英晶体频率为24MHz,但是SYSBOOT[15:14]为00,即选为19.2MHz,硬件引脚这样连接后,会有怎样的风险呢?

Other Parts Discussed in Thread: AM3354

AM3354,OSC0硬件设计石英晶体频率为24MHz,但是SYSBOOT[15:14]为00,即选为19.2MHz,如果这样设置的话,那通过ADPLLS、ADPLLLJ输出的CORE_CLKOUTM6、CORE_CLKOUTM4、CORE_CLKOUTM5、PER_CLKOUTM2等时钟输出会不会受影响呢?目前串口是可以正常通信,想知道硬件引脚这样连接会不会有风险呢?

  • 有人能帮我解答一下吗?目前我们的硬件没有将SYSBOOT[14]引脚拉高,那这样的话,就是选择了19.2MHz模式,而实际上外部晶振为24MHz,目前系统可以正常运行,串口、sd卡也都可以正常工作,但不知道这样系统时钟会不会受影响呢?比如串口的时钟为48MHz,那现在模式选择为19.2MHz后,串口的时钟是不是还是48MHz了呢?

  • 会有影响,我又客户搞错了这个,出现过问题,所以请您修改硬件。

  • Qin工:

       首先,非常感谢您的回答。然后我还有几个问题咨询一下,还请麻烦帮我回复一下:

         我想问下,如果我不想改硬件,想在软件上,强制认为目前就是SYSBOOT[15:14]的值就是01,可以实现吗?这个SYSBOOT[15:14]的判断应该不是在u-boot的代码里面吧?是在第一级引导ROM代码里面呢?能修改ROM代码实现我上面所说的功能吗?