This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 u-boot(2014.07)启动linux内核(3.14.43)到"Starting kernel ..."卡住



各位好:

    现在碰到u-boot启动内核在“Starting kernel ...”,跳到内核就没有打印信息输出了。请各位帮忙分析下。

环境如下:

1、SDK版本:ti-processor-sdk-linux-am335x-evm-01.00.00.03-Linux-x86-Install.bin

2、交叉编译环境宿主机器:Ubuntu LTS Server 14.04.2 32位

3、内核使用make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- zImage命令编译,.config文件参考附件

4、u-boot使用make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- O=am335x_evm am335x_evm_config all编译,把我司的板子环境变量当作AM335X_SK,即在read_eeprom中直接给am335x_baseboard_id结构赋值成AM35X的参数

5、我的板通过UART0串口输出

6、TI Demo板内存256M,我司板内存1G

 

操作步骤:

1、使用SDK自带的制作SD卡脚本,制作SD卡启动

2、修改u-boot/kernel

      a)根据我司板的具体硬件环境,修改内存初始化部分,屏蔽暂时没有的硬件初始化代码

      b)u-boot的MACH_TYPE_TIAM335EVM修改成和内核一致(4116)

      c)确定启动cmdline:console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait (UART0输出调试)

     d)编译内核menuconfig,选择“Kernel hacking”中选择“Kernel low-level debugging message via AM33XX UART1)”--选项中没有UART0,但是根据dts文件uart0设备的名字是UART1,不知道这样理解是否正确。

2、将编译好的内核和MLO/u-boot.img分别放入到SD卡的文件系统分区(/dev/mmcblk0p1)和启动分区中(/dev/mmcblk0p2 )

3、插入SD卡,启动

同一个内核文件,在TI Demo板上启动信息截取如下:

### main_loop: bootcmd="run findfdt; run mmcboot;setenv mmcdev 1; setenv bootpart 1:2; run mmcboot;run nandboot;"
Hit any key to stop autoboot:  0
test(4): 'A335X_SK' '=' 'A335BONE': returns 1
Command failed, result=1test(4): 'A335X_SK' '=' 'A335BNLT': returns 1
Command failed, result=1test(4): 'A335X_SK' '=' 'A33515BB': returns 1
Command failed, result=1test(4): 'A335X_SK' '=' 'A335X_SK': returns 0
Initial value for argc=3
Final value for argc=3
test(4): 'am335x-evmsk.dtb' '=' 'undefined': returns 1
Command failed, result=1Command failed, result=1mmc_init: 0, time 81
switch to partitions #0, OK
mmc0 is current device
mmc_init: 0, time 81
SD/MMC found on device 0
reading uEnv.txt
VFAT Support enabled
FAT32, fat_sect: 32, fatlength: 1112
Rootdir begins at cluster: 2, sector: 2256, offset: 11a000
Data begins at: 2254
Sector size: 512, cluster size: 1
FAT read sect=2256, clust_size=1, DIRENTSPERBLOCK=16
Rootvfatname: |pointercal|
RootMismatch: |pointe~1|pointercal|
RootMismatch: |pointe~1||
Rootvfatname: |000000000000u-boot.img|
RootMismatch: |000000~1.img|000000000000u-boot.img|
RootMismatch: |000000~1.img||
RootMismatch: |mlo||
Rootvfatname: |000000000000mlo|
RootMismatch: |000000~1|000000000000mlo|
RootMismatch: |000000~1||
Rootvfatname: |.ipaddr|
RootMismatch: |ipaddr~1|.ipaddr|
RootMismatch: |ipaddr~1||
Rootvfatname: |111u-boot.img|
RootMismatch: |111u-b~1.img|111u-boot.img|
RootMismatch: |111u-b~1.img||
END LOOP: j=0   clust_size=1
FAT read sect=2265, clust_size=1, DIRENTSPERBLOCK=16
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
END LOOP: j=0   clust_size=1
** Unable to read file uEnv.txt **
Command failed, result=1Command failed, result=1Command failed, result=1EXT2 rev 1, inode_size 256
ext4fs read 0 group descriptor (blkno 1 blkoff 0)
Iterate dir boot
iterate >.<
iterate >..<
iterate >bin<
iterate >boot<
Iterate dir zImage
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
iterate >.<
iterate >..<
iterate >zImage<
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
Got symlink >zImage-3.14.43-g875c69b<
Iterate dir zImage-3.14.43-g875c69b
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
iterate >.<
iterate >..<
iterate >zImage<
iterate >am335x-evm.dtb<
iterate >am335x-bone.dtb<
iterate >zImage-3.14.43-g875c69b<
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
4157920 bytes read in 300 ms (13.2 MiB/s)
Initial value for argc=3
Final value for argc=3
Initial value for argc=7
Final value for argc=7
test(4): 'try' '=' 'yes': returns 1
Command failed, result=1test(4): 'try' '=' 'try': returns 0
EXT2 rev 1, inode_size 256
ext4fs read 0 group descriptor (blkno 1 blkoff 0)
Iterate dir boot
iterate >.<
iterate >..<
iterate >bin<
iterate >boot<
Iterate dir am335x-evmsk.dtb
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
iterate >.<
iterate >..<
iterate >zImage<
iterate >am335x-evm.dtb<
iterate >am335x-bone.dtb<
iterate >zImage-3.14.43-g875c69b<
iterate >devicetree-zImage-am335x-evm.dtb<
iterate >am335x-evmsk.dtb<
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
Got symlink >devicetree-zImage-am335x-evmsk.dtb<
Iterate dir devicetree-zImage-am335x-evmsk.dtb
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
iterate >.<
iterate >..<
iterate >zImage<
iterate >am335x-evm.dtb<
iterate >am335x-bone.dtb<
iterate >zImage-3.14.43-g875c69b<
iterate >devicetree-zImage-am335x-evm.dtb<
iterate >am335x-evmsk.dtb<
iterate >devicetree-zImage-am335x-boneblack.dtb<
iterate >devicetree-zImage-am335x-bone.dtb<
iterate >devicetree-zImage-am335x-evmsk.dtb<
ext4fs read 5 group descriptor (blkno 1 blkoff 160)
36445 bytes read in 120 ms (295.9 KiB/s)
Initial value for argc=3
Final value for argc=3
entry >>> bootz_start  argv[1]=->>>
   Image Name:  
   Created:      1970-01-01   0:00:00 UTC
   Image Type:   Invalid ARCH Invalid OS Invalid Image (uncompressed)
   Data Size:    0 Bytes = 0 Bytes
   Load Address: 00000000
   Entry Point:  00000000
entry >>> bootm_start >>>
## Current stack ends at 0x8e715890 *  kernel: cmdline image address = 0x82000000
Kernel image @ 0x82000000 [ 0x000000 - 0x3f71e0 ]
entry >>> bootm_find_ramdisk >>>
entry >>> boot_get_ramdisk >>>
## Skipping init Ramdisk
## No init Ramdisk
   ramdisk start = 0x00000000, ramdisk end = 0x00000000
*  fdt: cmdline image address = 0x88000000
## Checking for 'FDT'/'FDT Image' at 88000000
Wrong FIT format: no description
*  fdt: raw FDT blob
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   of_flat_tree at 0x88000000 size 0x00008e5d
Initial value for argc=3
Final value for argc=3
using: FDT
## initrd_high = 0xffffffff, copy_to_ram = 1
   ramdisk load start = 0x00000000, ramdisk load end = 0x00000000
## device tree at 88000000 ... 88008e5c (len=48733 [0xBE5D])
   Loading Device Tree to 8e708000, end 8e713e5c ... OK
Initial value for argc=3
Final value for argc=3
Updating property '/ocp/ethernet@4a100000/slave@4a100200/mac-address' =  c4 ed ba 8b 33 fd
Updating property '/ocp/ethernet@4a100000/slave@4a100200/local-mac-address' =  c4 ed ba 8b 33 fd
Updating property '/ocp/ethernet@4a100000/slave@4a100300/mac-address' =  c4 ed ba 8b 33 ff
Updating property '/ocp/ethernet@4a100000/slave@4a100300/local-mac-address' =  c4 ed ba 8b 33 ff
entry >>> boot_jump_linux >>>
flag=0x00000400,fake=0

   Image Name:  
   Created:      1970-01-01   0:00:00 UTC
   Image Type:   Invalid ARCH Invalid OS Invalid Image (uncompressed)
   Data Size:    0 Bytes = 0 Bytes
   Load Address: 00000000
   Entry Point:  00000000
##3 Transferring control to Linux (at address 82000000)...

Starting kernel ...

in boot_jump_linux addr=0x82000000
[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 3.14.43-g875c69b (root@mark) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #2 Sat Nov 14 18:04:41 CST 2015
[    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] Machine model: TI AM335x EVM-SK
[    0.000000] cma: CMA: reserved 24 MiB at 8c800000
[    0.000000] Memory policy: Data cache writeback
[    0.000000] CPU: All CPU(s) started in SVC mode.
[    0.000000] AM335X ES2.1 (sgx neon )
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait

在我司板启动信息如下:

### main_loop: bootcmd="run findfdt; run mmcboot;setenv mmcdev 1; setenv bootpart 1:2; run mmcboot;run nandboot;"
Hit any key to stop autoboot:  0
test(4): 'A335X_SK' '=' 'A335BONE': returns 1
Command failed, result=1test(4): 'A335X_SK' '=' 'A335BNLT': returns 1
Command failed, result=1test(4): 'A335X_SK' '=' 'A33515BB': returns 1
Command failed, result=1test(4): 'A335X_SK' '=' 'A335X_SK': returns 0
test(4): 'am335x-evmsk.dtb' '=' 'undefined': returns 1
Command failed, result=1Command failed, result=1mmc_init: 0, time 77
switch to partitions #0, OK
mmc0 is current device
mmc_init: 0, time 77
SD/MMC found on device 0
reading uEnv.txt
VFAT Support enabled
FAT32, fat_sect: 32, fatlength: 1112
Rootdir begins at cluster: 2, sector: 2256, offset: 11a000
Data begins at: 2254
Sector size: 512, cluster size: 1
FAT read sect=2256, clust_size=1, DIRENTSPERBLOCK=16
RootMismatch: |mlo||
Rootvfatname: |u-boot.img|
RootMismatch: |u-boot.img|u-boot.img|
RootMismatch: |u-boot.img||
END LOOP: j=0   clust_size=1
** Unable to read file uEnv.txt **
Command failed, result=1Command failed, result=1Command failed, result=1EXT2 rev 1, inode_size 256
ext4fs read 0 group descriptor (blkno 1 blkoff 0)
Iterate dir boot
iterate >.<
iterate >..<
iterate >bin<
iterate >dev<
iterate >sys<
iterate >lib<
iterate >srv<
iterate >mnt<
iterate >proc<
iterate >boot<
Iterate dir zImage
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
iterate >.<
iterate >..<
iterate >am335x-bone.dtb<
iterate >zImage-3.14.43-g875c69b<
iterate >am335x-evmsk.dtb<
iterate >zImage<
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
Got symlink >zImage-3.14.43-g875c69b<
Iterate dir zImage-3.14.43-g875c69b
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
iterate >.<
iterate >..<
iterate >am335x-bone.dtb<
iterate >zImage-3.14.43-g875c69b<
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
4157920 bytes read in 463 ms (8.6 MiB/s)
test(4): 'try' '=' 'yes': returns 1
Command failed, result=1test(4): 'try' '=' 'try': returns 0
EXT2 rev 1, inode_size 256
ext4fs read 0 group descriptor (blkno 1 blkoff 0)
Iterate dir boot
iterate >.<
iterate >..<
iterate >bin<
iterate >dev<
iterate >sys<
iterate >lib<
iterate >srv<
iterate >mnt<
iterate >proc<
iterate >boot<
Iterate dir am335x-evmsk.dtb
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
iterate >.<
iterate >..<
iterate >am335x-bone.dtb<
iterate >zImage-3.14.43-g875c69b<
iterate >am335x-evmsk.dtb<
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
Got symlink >devicetree-zImage-am335x-evmsk.dtb<
Iterate dir devicetree-zImage-am335x-evmsk.dtb
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
iterate >.<
iterate >..<
iterate >am335x-bone.dtb<
iterate >zImage-3.14.43-g875c69b<
iterate >am335x-evmsk.dtb<
iterate >zImage<
iterate >am335x-evm.dtb<
iterate >devicetree-zImage-am335x-evm.dtb<
iterate >devicetree-zImage-am335x-boneblack.dtb<
iterate >am335x-boneblack.dtb<
iterate >devicetree-zImage-am335x-bone.dtb<
iterate >devicetree-zImage-am335x-evmsk.dtb<
ext4fs read 10 group descriptor (blkno 1 blkoff 320)
36445 bytes read in 138 ms (257.8 KiB/s)
entry >>> bootz_start  argv[1]=->>>
   Image Name:  
   Created:      1970-01-01   0:00:00 UTC
   Image Type:   Invalid ARCH Invalid OS Invalid Image (uncompressed)
   Data Size:    0 Bytes = 0 Bytes
   Load Address: 00000000
   Entry Point:  00000000
entry >>> bootm_start >>>
## Current stack ends at 0xbe714890 *  kernel: cmdline image address = 0x82000000
Kernel image @ 0x82000000 [ 0x000000 - 0x3f71e0 ]
entry >>> bootm_find_ramdisk >>>
entry >>> boot_get_ramdisk >>>
## Skipping init Ramdisk
## No init Ramdisk
   ramdisk start = 0x00000000, ramdisk end = 0x00000000
*  fdt: cmdline image address = 0x88000000
## Checking for 'FDT'/'FDT Image' at 88000000
Wrong FIT format: no description
*  fdt: raw FDT blob
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   of_flat_tree at 0x88000000 size 0x00008e5d
using: FDT
## initrd_high = 0xffffffff, copy_to_ram = 1
   ramdisk load start = 0x00000000, ramdisk load end = 0x00000000
## device tree at 88000000 ... 88008e5c (len=48733 [0xBE5D])
   Loading Device Tree to 8fff4000, end 8ffffe5c ... OK
Updating property '/ocp/ethernet@4a100000/slave@4a100200/mac-address' =  00 84 00 16 05 05
Updating property '/ocp/ethernet@4a100000/slave@4a100200/local-mac-address' =  00 84 00 16 05 05
Updating property '/ocp/ethernet@4a100000/slave@4a100300/mac-address' =  00 16 84 00 05 02
Updating property '/ocp/ethernet@4a100000/slave@4a100300/local-mac-address' =  00 16 84 00 05 02
entry >>> boot_jump_linux >>>
flag=0x00000400,fake=0

##3 Transferring control to Linux (machid=0x00001014(4116) at address 82000000)...

Starting kernel ...

console=ttyO0,115200n8 root=/dev/mmcblk0p2 ro rootfstype=ext4 rootwait

in boot_jump_linux addr=0x82000000  r2=0x8fff4000

后面就没有信息了。在TI Demo板和我司板的u-boot中,在boot_jump_linux 函数中,将起始地址为0x82000000开始,64K长度的内存数据都打印出来,两个板的一样。