This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807 AP设置不成功



我们的方案是把wl1807的AP路由到ppp0网口,使得手机可以接入该AP上网。

经过测试我们的ppp0网络连接正常。wl1807设置成AP后,手机能接入该AP但是不能上网。以下是我们AP的设置方法:

说明:我们用的SDK是ti-processor-sdk-linux-am335x-evm-01.00.00.00,内核版本linux3.14.26。以下驱动均从ti-processor-sdk-linux-am335x-evm-01.00.00.00/board-support/extra-drivers/ti-compat-wireless-wl18xx-R8.5编译而来:

cfg80211.ko      

mac80211.ko      

wl18xx.ko
compat.ko

wlcore.ko
wlcore_sdio.ko

安装驱动后出现

] D:chip id 0x6030111 (185x PG20)
[  639.258486] D:base address: oui 5c313e nic e1a8ab
[  639.268775] wlcore: loaded
[  639.272265] wlcore: driver version: ol_r8.a9.14
[  639.277045] wlcore: compilation time: Wed Nov  4 10:25:59 2015

接着就直接设置AP.使用的脚本是usr/share/wl18xx/ap_start.sh:(绿色部分是我自己修改的)

#!/bin/sh

########## variables ##########

WLAN=wlan1
HOSTAPD_GLOBAL=/var/run/hostapd_global
HOSTAPD_CONF=/usr/share/wl18xx/hostapd.conf
IP_ADDR=192.168.43.1
DHCP_CONF=udhcpd.conf
DHCP_CONF_PROC=u[d]hcpd.conf

########## body ##########

### check for configuration file---------------------------hostapd.conf
##if /usr/share/wl18xx/hostapd.conf not exist and wlan name is wlan2,then print error - no default hostapd.conf for wlan1
if [ ! -f $HOSTAPD_CONF ] && [ $WLAN == "wlan2" ]; then
 echo "error - no default hostapd.conf for $WLAN"
 exit 1
else
##else chmod 777 /usr/share/wl18xx/hostapd.conf
 chmod 777 $HOSTAPD_CONF
fi

##if /usr/share/wl18xx/hostapd.conf is not exitsted and wlan name is wlan1,and if also /etc/hostapd.conf not existed,print error
if [ ! -f $HOSTAPD_CONF ] && [ $WLAN == "wlan1" ]; then
 if [ ! -f /etc/hostapd.conf ]
 then
  echo "error - no default hostapd.conf for $WLAN"
  exit 1
 fi
## if /etc/hostapd.conf existed ,copy the file to /usr/share/wl18xx/hostapd.conf
 cp /etc/hostapd.conf $HOSTAPD_CONF
 chmod 777 $HOSTAPD_CONF
fi


### configure ip forewarding-----------------enable ip routing
echo 1 > /proc/sys/net/ipv4/ip_forward

### add WLAN interface, if not present
if [ ! -d /sys/class/net/$WLAN ]
then
  echo "adding $WLAN interface"
  iw phy `ls /sys/class/ieee80211/` interface add $WLAN type managed
fi

### start a hostapd global control interface, if not present
if [ ! -r $HOSTAPD_GLOBAL ]
then
 hostapd -g $HOSTAPD_GLOBAL &
 sleep 1
fi

### add ap interface
hostapd_cli -g $HOSTAPD_GLOBAL raw ADD $WLAN config=$HOSTAPD_CONF enable=1

### configure ip
ifconfig $WLAN $IP_ADDR netmask 255.255.255.0 up

### start udhcpd server, if not started
output=`ps | grep /usr/share/wl18xx\$DHCP_CONF_PROC`
set -- $output
echo $output
if [ -z "$output" ]; then
 udhcpd $DHCP_CONF
fi

### configure nat
#iptables -t nat -A POSTROUTING -o eth0 -j MASQUERADE

iptables -t nat -A POSTROUTING -o eth0 -j MASQUERADE

iptables -A FORWARD -i ppp0 -o wlan0 -m state --state RELATED,ESTABLISHED -j ACCEPT
iptables -A FORWARD -i wlan0 -o ppp0 -j ACCEPT

/usr/share/wl18xx/hostapd.conf 是用sdk提供的文件系统中拷出来的。

/usr/share/wl18xx/udhcpd.conf是我自己改的(在另一款wifi设置中证明可行)内容是

interface wlan1
remain yes
opt dns 218.104.128.106  211.138.150.58 211.138.155.90
option subnet 255.255.255.0
option dns 211.138.150.58
opt router 192.168.43.1
option domain local
option lease 864000

以上是全部配置。可以连接上AP:SitaraAP 但是就是上不了网,在wlcore相关驱动中,我们打开wl1271_debug

在运行./ap_start.sh 后出现的信息是:

###configure ip forewarding............
adding wlan1 interface
### start a hosapd global control interface...............
###add ap interface...................
[  456.818711] D:mac80211 start
[  456.822429] D:mac80211 add interface type 3 mac 5c:31:3e:e1:a8:ac
[  456.828865] D:allocating hw queue base: 0
[  456.833123] wl12xx_init_fw....................
[  457.200001] D:mem_start 00700000 mem_size 0000030C
[  457.205048] D:reg_start 00802000 reg_size 00014578
[  457.210110] D:mem2_start 00B00404 mem2_size 00001000
[  457.215334] D:mem3_start 00C00000 mem3_size 00000400
[  457.221255] D:booting firmware ti-connectivity/wl18xx-fw-4.bin
[  457.315089] D:mem_start 00A02000 mem_size 00010000
[  457.320289] D:reg_start 00807000 reg_size 00005000
[  457.325332] D:mem2_start 00800000 mem2_size 0000B000
[  457.330572] D:mem3_start 00000000 mem3_size 00000000
[  457.336835] D:clock freq 5 (13, 120, 0, 0, spit)
[  457.344532] D:mem_start 00700000 mem_size 0000030C
[  457.349574] D:reg_start 00802000 reg_size 00014578
[  457.354639] D:mem2_start 00B00404 mem2_size 00001000
[  457.359855] D:mem3_start 00C00000 mem3_size 00000400
[  457.365661] D:mem_start 00700000 mem_size 0000030C
[  457.370720] D:reg_start 00802000 reg_size 00014578
[  457.375760] D:mem2_start 00B00404 mem2_size 00001000
[  457.380996] D:mem3_start 00C00000 mem3_size 00000400
[  457.387261] D:chip id 0x6030111
[  457.390779] D:mem_start 80926000 mem_size 00016A44
[  457.395817] D:reg_start 00000000 reg_size 00000000
[  457.400875] D:mem2_start 00000000 mem2_size 00000000
[  457.406098] D:mem3_start 00000000 mem3_size 00000000
[  457.411881] D:firmware chunks to be uploaded: 15
[  457.416741] D:chunk 14 addr 0x0 len 101320
[  457.421061] D:starting firmware upload
[  457.425002] D:fw_data_len 101320 chunk_size 16384
[  457.430724] D:mem_start 00000000 mem_size 00014000
[  457.435763] D:reg_start 00810000 reg_size 0000BFFF
[  457.440831] D:mem2_start 00000000 mem2_size 00000000
[  457.446049] D:mem3_start 00000000 mem3_size 00000000
[  457.451798] D:uploading fw chunk 0xc5d1800c to 0x0
[  457.457713] D:uploading fw chunk 0xc5d1c00c to 0x4000
[  457.464132] D:uploading fw chunk 0xc5d2000c to 0x8000
[  457.470361] D:uploading fw chunk 0xc5d2400c to 0xc000
[  457.476473] D:mem_start 00010000 mem_size 00014000
[  457.481541] D:reg_start 00810000 reg_size 0000BFFF
[  457.486576] D:mem2_start 00000000 mem2_size 00000000
[  457.491809] D:mem3_start 00000000 mem3_size 00000000
[  457.497618] D:uploading fw chunk 0xc5d2800c to 0x10000
[  457.504510] D:uploading fw chunk 0xc5d2c00c to 0x14000
[  457.510744] D:uploading fw last chunk (3016 B) 0xc5d3000c to 0x18000
[  457.517626] D:chunk 13 addr 0x100000 len 131072
[  457.522416] D:starting firmware upload
[  457.526357] D:fw_data_len 131072 chunk_size 16384
[  457.531483] D:mem_start 00100000 mem_size 00014000
[  457.536524] D:reg_start 00810000 reg_size 0000BFFF
[  457.541578] D:mem2_start 00000000 mem2_size 00000000
[  457.546794] D:mem3_start 00000000 mem3_size 00000000
[  457.553070] D:mem_start 00100000 mem_size 00014000
[  457.558117] D:reg_start 00810000 reg_size 0000BFFF
[  457.563178] D:mem2_start 00000000 mem2_size 00000000
[  457.568395] D:mem3_start 00000000 mem3_size 00000000
[  457.574122] D:uploading fw chunk 0xc5d30bdc to 0x100000
[  457.580412] D:mem_start 00104000 mem_size 00014000
[  457.585451] D:reg_start 00810000 reg_size 0000BFFF
[  457.590517] D:mem2_start 00000000 mem2_size 00000000
[  457.595737] D:mem3_start 00000000 mem3_size 00000000
[  457.601486] D:uploading fw chunk 0xc5d34bdc to 0x104000
[  457.607774] D:mem_start 00108000 mem_size 00014000
[  457.612858] D:reg_start 00810000 reg_size 0000BFFF
[  457.617889] D:mem2_start 00000000 mem2_size 00000000
[  457.623121] D:mem3_start 00000000 mem3_size 00000000
[  457.628836] D:uploading fw chunk 0xc5d38bdc to 0x108000
[  457.635637] D:mem_start 0010C000 mem_size 00014000
[  457.640714] D:reg_start 00810000 reg_size 0000BFFF
[  457.645751] D:mem2_start 00000000 mem2_size 00000000
[  457.650985] D:mem3_start 00000000 mem3_size 00000000
[  457.656703] D:uploading fw chunk 0xc5d3cbdc to 0x10c000
[  457.663489] D:mem_start 00110000 mem_size 00014000
[  457.668531] D:reg_start 00810000 reg_size 0000BFFF
[  457.673585] D:mem2_start 00000000 mem2_size 00000000
[  457.678798] D:mem3_start 00000000 mem3_size 00000000
[  457.684517] D:uploading fw chunk 0xc5d40bdc to 0x110000
[  457.691288] D:mem_start 00114000 mem_size 00014000
[  457.696324] D:reg_start 00810000 reg_size 0000BFFF
[  457.701396] D:mem2_start 00000000 mem2_size 00000000
[  457.706621] D:mem3_start 00000000 mem3_size 00000000
[  457.712355] D:uploading fw chunk 0xc5d44bdc to 0x114000
[  457.718642] D:mem_start 00118000 mem_size 00014000
[  457.723708] D:reg_start 00810000 reg_size 0000BFFF
[  457.728742] D:mem2_start 00000000 mem2_size 00000000
[  457.733975] D:mem3_start 00000000 mem3_size 00000000
[  457.739701] D:uploading fw chunk 0xc5d48bdc to 0x118000
[  457.746504] D:mem_start 0011C000 mem_size 00014000
[  457.751569] D:reg_start 00810000 reg_size 0000BFFF
[  457.756606] D:mem2_start 00000000 mem2_size 00000000
[  457.761833] D:mem3_start 00000000 mem3_size 00000000
[  457.767564] D:uploading fw chunk 0xc5d4cbdc to 0x11c000
[  457.774407] D:uploading fw last chunk (0 B) 0xc5d50bdc to 0x120000
[  457.781089] D:chunk 12 addr 0x20400000 len 53692
[  457.785946] D:starting firmware upload
[  457.789882] D:fw_data_len 53692 chunk_size 16384
[  457.795035] D:mem_start 20400000 mem_size 00014000
[  457.800103] D:reg_start 00810000 reg_size 0000BFFF
[  457.805143] D:mem2_start 00000000 mem2_size 00000000
[  457.810369] D:mem3_start 00000000 mem3_size 00000000
[  457.816014] D:mem_start 20400000 mem_size 00014000
[  457.821077] D:reg_start 00810000 reg_size 0000BFFF
[  457.826108] D:mem2_start 00000000 mem2_size 00000000
[  457.831341] D:mem3_start 00000000 mem3_size 00000000
[  457.837622] D:uploading fw chunk 0xc5d50be4 to 0x20400000
[  457.844296] D:mem_start 20404000 mem_size 00014000
[  457.849335] D:reg_start 00810000 reg_size 0000BFFF
[  457.854395] D:mem2_start 00000000 mem2_size 00000000
[  457.859606] D:mem3_start 00000000 mem3_size 00000000
[  457.865364] D:uploading fw chunk 0xc5d54be4 to 0x20404000
[  457.872329] D:mem_start 20408000 mem_size 00014000
[  457.877368] D:reg_start 00810000 reg_size 0000BFFF
[  457.882432] D:mem2_start 00000000 mem2_size 00000000
[  457.887651] D:mem3_start 00000000 mem3_size 00000000
[  457.893392] D:uploading fw chunk 0xc5d58be4 to 0x20408000
[  457.899899] D:uploading fw last chunk (4540 B) 0xc5d5cbe4 to 0x2040c000
[  457.907329] D:chunk 11 addr 0xb00000 len 496
[  457.911840] D:starting firmware upload
[  457.915777] D:fw_data_len 496 chunk_size 16384
[  457.920606] D:mem_start 00B00000 mem_size 00014000
[  457.925643] D:reg_start 00810000 reg_size 0000BFFF
[  457.930702] D:mem2_start 00000000 mem2_size 00000000
[  457.935916] D:mem3_start 00000000 mem3_size 00000000
[  457.942036] D:uploading fw last chunk (496 B) 0xc5d5dda8 to 0xb00000
[  457.948808] D:chunk 10 addr 0xb0ae40 len 28512
[  457.953504] D:starting firmware upload
[  457.957445] D:fw_data_len 28512 chunk_size 16384
[  457.962462] D:mem_start 00B0AE40 mem_size 00014000
[  457.967498] D:reg_start 00810000 reg_size 0000BFFF
[  457.972556] D:mem2_start 00000000 mem2_size 00000000
[  457.977775] D:mem3_start 00000000 mem3_size 00000000
[  457.984001] D:mem_start 00B0AE40 mem_size 00014000
[  457.989042] D:reg_start 00810000 reg_size 0000BFFF
[  457.994100] D:mem2_start 00000000 mem2_size 00000000
[  457.999316] D:mem3_start 00000000 mem3_size 00000000
[  458.005050] D:uploading fw chunk 0xc5d5dfa0 to 0xb0ae40
[  458.011892] D:uploading fw last chunk (12128 B) 0xc5d61fa0 to 0xb0ee40
[  458.019376] D:chunk 9 addr 0x80900000 len 60120
[  458.024169] D:starting firmware upload
[  458.028107] D:fw_data_len 60120 chunk_size 16384
[  458.033140] D:mem_start 80900000 mem_size 00014000
[  458.038178] D:reg_start 00810000 reg_size 0000BFFF
[  458.043242] D:mem2_start 00000000 mem2_size 00000000
[  458.048462] D:mem3_start 00000000 mem3_size 00000000
[  458.054768] D:uploading fw chunk 0xc5d64f08 to 0x80900000
[  458.061527] D:uploading fw chunk 0xc5d68f08 to 0x80904000
[  458.068086] D:uploading fw chunk 0xc5d6cf08 to 0x80908000
[  458.074945] D:uploading fw last chunk (10968 B) 0xc5d70f08 to 0x8090c000
[  458.082791] D:chunk 8 addr 0x80920000 len 31652
[  458.087559] D:starting firmware upload
[  458.091530] D:fw_data_len 31652 chunk_size 16384
[  458.096532] D:mem_start 80920000 mem_size 00014000
[  458.101596] D:reg_start 00810000 reg_size 0000BFFF
[  458.106634] D:mem2_start 00000000 mem2_size 00000000
[  458.111875] D:mem3_start 00000000 mem3_size 00000000
[  458.118075] D:uploading fw chunk 0xc5d739e8 to 0x80920000
[  458.124819] D:uploading fw last chunk (15268 B) 0xc5d779e8 to 0x80924000
[  458.132855] D:chunk 7 addr 0x80940000 len 6144
[  458.137524] D:starting firmware upload
[  458.141488] D:fw_data_len 6144 chunk_size 16384
[  458.146406] D:mem_start 80940000 mem_size 00014000
[  458.151467] D:reg_start 00810000 reg_size 0000BFFF
[  458.156504] D:mem2_start 00000000 mem2_size 00000000
[  458.161736] D:mem3_start 00000000 mem3_size 00000000
[  458.167875] D:uploading fw last chunk (6144 B) 0xc5d7b594 to 0x80940000
[  458.175332] D:chunk 6 addr 0x80944000 len 6144
[  458.180027] D:starting firmware upload
[  458.183965] D:fw_data_len 6144 chunk_size 16384
[  458.188862] D:mem_start 80944000 mem_size 00014000
[  458.193925] D:reg_start 00810000 reg_size 0000BFFF
[  458.198957] D:mem2_start 00000000 mem2_size 00000000
[  458.204189] D:mem3_start 00000000 mem3_size 00000000
[  458.210380] D:uploading fw last chunk (6144 B) 0xc5d7cd9c to 0x80944000
[  458.217646] D:chunk 5 addr 0x80948000 len 6144
[  458.222345] D:starting firmware upload
[  458.226281] D:fw_data_len 6144 chunk_size 16384
[  458.231219] D:mem_start 80948000 mem_size 00014000
[  458.236255] D:reg_start 00810000 reg_size 0000BFFF
[  458.241315] D:mem2_start 00000000 mem2_size 00000000
[  458.246527] D:mem3_start 00000000 mem3_size 00000000
[  458.252769] D:uploading fw last chunk (6144 B) 0xc5d7e5a4 to 0x80948000
[  458.260154] D:chunk 4 addr 0x8094c000 len 6144
[  458.264828] D:starting firmware upload
[  458.268765] D:fw_data_len 6144 chunk_size 16384
[  458.273817] D:mem_start 8094C000 mem_size 00014000
[  458.278851] D:reg_start 00810000 reg_size 0000BFFF
[  458.283911] D:mem2_start 00000000 mem2_size 00000000
[  458.289129] D:mem3_start 00000000 mem3_size 00000000
[  458.294824] D:uploading fw last chunk (6144 B) 0xc5d7fdac to 0x8094c000
[  458.302583] D:chunk 3 addr 0x80950000 len 8192
[  458.307252] D:starting firmware upload
[  458.311215] D:fw_data_len 8192 chunk_size 16384
[  458.316120] D:mem_start 80950000 mem_size 00014000
[  458.321185] D:reg_start 00810000 reg_size 0000BFFF
[  458.326220] D:mem2_start 00000000 mem2_size 00000000
[  458.331446] D:mem3_start 00000000 mem3_size 00000000
[  458.337576] D:uploading fw last chunk (8192 B) 0xc5d815b4 to 0x80950000
[  458.345127] D:chunk 2 addr 0x80960000 len 20656
[  458.349890] D:starting firmware upload
[  458.353852] D:fw_data_len 20656 chunk_size 16384
[  458.358846] D:mem_start 80960000 mem_size 00014000
[  458.363908] D:reg_start 00810000 reg_size 0000BFFF
[  458.368940] D:mem2_start 00000000 mem2_size 00000000
[  458.374178] D:mem3_start 00000000 mem3_size 00000000
[  458.380372] D:uploading fw chunk 0xc5d835bc to 0x80960000
[  458.386879] D:uploading fw last chunk (4272 B) 0xc5d875bc to 0x80964000
[  458.394387] D:chunk 1 addr 0x80953000 len 1536
[  458.399058] D:starting firmware upload
[  458.403022] D:fw_data_len 1536 chunk_size 16384
[  458.407931] D:mem_start 80953000 mem_size 00014000
[  458.412988] D:reg_start 00810000 reg_size 0000BFFF
[  458.418018] D:mem2_start 00000000 mem2_size 00000000
[  458.423243] D:mem3_start 00000000 mem3_size 00000000
[  458.429380] D:uploading fw last chunk (1536 B) 0xc5d88674 to 0x80953000
[  458.436620] D:chunk 0 addr 0x80958000 len 24576
[  458.441408] D:starting firmware upload
[  458.445351] D:fw_data_len 24576 chunk_size 16384
[  458.450364] D:mem_start 80958000 mem_size 00014000
[  458.455398] D:reg_start 00810000 reg_size 0000BFFF
[  458.460462] D:mem2_start 00000000 mem2_size 00000000
[  458.465675] D:mem3_start 00000000 mem3_size 00000000
[  458.471923] D:uploading fw chunk 0xc5d88c7c to 0x80958000
[  458.478416] D:uploading fw last chunk (8192 B) 0xc5d8cc7c to 0x8095c000
[  458.486084] D:mem_start 80926000 mem_size 00016A44
[  458.491148] D:reg_start 00000000 reg_size 00000000
[  458.496178] D:mem2_start 00000000 mem2_size 00000000
[  458.501410] D:mem3_start 00000000 mem3_size 00000000
[  458.507161] D:mem_start 00700000 mem_size 0000030C
[  458.512233] D:reg_start 00802000 reg_size 00014578
[  458.517265] D:mem2_start 00B00404 mem2_size 00001000
[  458.522499] D:mem3_start 00C00000 mem3_size 00000400
[  458.528805] D:chip id after firmware boot: 0x6030111
[  458.550002] D:cmd_box_addr 0xb007f8
[  458.553711] D:MBOX ptrs: 0xb00adc 0xb00b90
[  458.558075] wlcore: PHY firmware version: Rev 8.2.0.0.224
[  458.563773] D:unmasking event_mask 0xffef01
[  458.568170] D:acx event mbox mask
[  458.571827] D:cmd configure (17)
[  458.575505] D:mem_start 00800000 mem_size 000050FC
[  458.580569] D:reg_start 00B00404 reg_size 00001000
[  458.585603] D:mem2_start 00C00000 mem2_size 00000400
[  458.590831] D:mem3_start 00000000 mem3_size 00000000
[  458.597501] D:acx cfg bitmap 89 blk 256 spare 1 field 15
[  458.603271] D:cmd configure (57)
[  458.606970] D:cmd template_set 2 (role 255)
[  458.611950] D:cmd template_set 3 (role 255)
[  458.616672] D:cmd template_set 19 (role 255)
[  458.621757] D:cmd template_set 20 (role 255)
[  458.626567] D:cmd template_set 0 (role 255)
[  458.631549] D:cmd template_set 6 (role 255)
[  458.636273] D:cmd template_set 5 (role 255)
[  458.641255] D:cmd template_set 4 (role 255)
[  458.645973] D:cmd template_set 1 (role 255)
[  458.650946] D:cmd template_set 15 (role 255)
[  458.655751] D:cmd template_set 14 (role 255)
[  458.660841] D:cmd template_set 13 (role 255)
[  458.665654] D:cmd template_set 16 (role 255)
[  458.670731] D:cmd template_set 7 (role 255)
[  458.675455] D:cmd template_set 7 (role 255)
[  458.680418] D:cmd template_set 7 (role 255)
[  458.685136] D:cmd template_set 7 (role 255)
[  458.689849] D:wl1271 mem cfg
[  458.693171] D:cmd configure (1)
[  458.697018] D:cmd config firmware logger
[  458.703070] D:cmd reg domain config
[  458.706786] D:cmd reg domain bitmap1: 0x000007ff, bitmap2: 0x00000000
[  458.783237] D:acx sg cfg
[  458.785920] D:cmd configure (22)
[  458.810091] D:acx sg enable
[  458.813038] D:cmd configure (21)
[  458.816667] D:acx mem map
[  458.819419] D:cmd interrogate
[  458.823232] D:available tx blocks: 44
[  458.827086] D:acx rx msdu life time
[  458.830991] D:cmd configure (60)
[  458.834637] D:acx dco itrim parameters
[  458.838580] D:cmd configure (55)
[  458.842508] D:acx tx config options
[  458.846178] D:cmd configure (15)
[  458.849848] D:wl1271 rx interrupt config
[  458.854268] D:cmd configure (39)
[  458.857958] D:acx cca threshold
[  458.861487] D:cmd configure (16)
[  458.865129] D:acx frag threshold: 2352
[  458.869067] D:cmd configure (40)
[  458.873030] D:cmd data path
[  458.876260] D:rx start cmd channel 1
[  458.880605] D:tx start cmd channel 1
[  458.884362] D:acx pm config
[  458.887296] D:cmd configure (64)
[  458.891298] D:acx set rate mgmt params
[  458.895244] D:cmd configure (52)
[  458.898869] D:acx config hangover
[  458.902655] D:cmd configure (66)
[  458.906387] wlcore: firmware booted (Rev 8.9.0.0.31)
[  458.911634] D:11a is supported
[  458.914839] #########################################
[  458.920159] wl12xx_cmd_role_enable................
[  458.925194] D:cmd role enable
[  458.928792] wl1271_init_vif_specific................
[  458.934038] D:acx sleep auth 2
[  458.937957] D:cmd configure (29)
[  458.941801] D:unmasking event_mask 0xffff01
[  458.946197] D:acx event mbox mask
[  458.949686] D:cmd configure (17)
[  458.953710] D:AP basic rate set: 0x1eff
[  458.957750] D:acx ap rate policy 0 rates 0x1eff
[  458.962743] D:cmd configure (27)
[  458.966438] D:acx ap rate policy 1 rates 0x1
[  458.971156] D:cmd configure (27)
[  458.974847] D:acx ap rate policy 2 rates 0x1ffeff
[  458.979790] D:cmd configure (27)
[  458.983768] D:acx ap rate policy 3 rates 0x1ffeff
[  458.988714] D:cmd configure (27)
[  458.992629] D:acx ap rate policy 4 rates 0x1ffeff
[  458.997579] D:cmd configure (27)
[  459.001772] D:acx ap rate policy 5 rates 0x1ffeff
[  459.006725] D:cmd configure (27)
[  459.010696] D:acx config ap sleep
[  459.014181] D:cmd configure (89)
[  459.017848] D:acx ap max tx retry
[  459.021640] D:cmd configure (58)
[  459.025332] D:acx dot11_cur_tx_pwr 0
[  459.029094] D:cmd configure (61)
[  459.033073] D:acx slot
[  459.035560] D:cmd configure (2)
[  459.039136] D:acx service period timeout
[  459.043285] D:cmd configure (33)
[  459.047406] D:acx rts threshold: 2353
[  459.051408] D:cmd configure (62)
[  459.055103] D:acx ac cfg 0 cw_ming 15 cw_max 63 aifs 3 txop 0
[  459.061375] D:cmd configure (3)
[  459.064965] D:acx tid config
[  459.067992] D:cmd configure (9)
[  459.071875] D:acx ac cfg 1 cw_ming 15 cw_max 63 aifs 7 txop 0
[  459.077920] D:cmd configure (3)
[  459.081739] D:acx tid config
[  459.084772] D:cmd configure (9)
[  459.088304] D:acx ac cfg 2 cw_ming 15 cw_max 63 aifs 1 txop 3008
[  459.094907] D:cmd configure (3)
[  459.098501] D:acx tid config
[  459.101750] D:cmd configure (9)
[  459.105344] D:acx ac cfg 3 cw_ming 15 cw_max 63 aifs 1 txop 1504
[  459.111886] D:cmd configure (3)
[  459.115470] D:acx tid config
[  459.118500] D:cmd configure (9)
[  459.122339] D:acx feature cfg
[  459.125464] D:cmd configure (67)
[  459.129132] D:cmd template_set 16 (role 0)
[  459.134076] D:cmd template_set 0 (role 0)
[  459.138619] D:cmd template_set 5 (role 0)
[  459.143461] D:acx beacon filter opt enable=0
[  459.147955] D:cmd configure (11)
[  459.151865] D:acx ba initiator policy
[  459.155722] D:cmd configure (46)
[  459.159388] list_add................
[  459.163174] wlvif->bss_type 3............
[  459.167412] D:IRQ work
[  459.169988] D:intr: 0x4 (fw_rx_counter = 0, drv_rx_counter = 0, tx_results_counter = 0)
[  459.178410] D:WL1271_ACX_INTR_EVENT_A
[  459.182271] D:EVENT on mbox 0
[  459.185443] D:MBOX vector: 0x80000
[  459.189157] D:intr: 0x0 (fw_rx_counter = 0, drv_rx_counter = 0, tx_results_counter = 0)
[  459.198312] D:mac80211 configure filter changed 180 total 80000180
[  459.204997] D:mac80211 bss info role 0 changed 0xe
[  459.210197] D:acx slot
[  459.212684] D:cmd configure (2)
[  459.216282] D:acx_set_preamble
[  459.219492] D:cmd configure (30)
[  459.223544] D:acx_set_ctsprotect
[  459.226940] D:cmd configure (28)
[  459.230890] D:mac80211 conf tx 0
[  459.234289] D:acx ac cfg 3 cw_ming 3 cw_max 7 aifs 2 txop 1504
[  459.240658] D:cmd configure (3)
[  459.244226] D:acx tid config
[  459.247254] D:cmd configure (9)
[  459.251114] D:mac80211 conf tx 1
[  459.254516] D:acx ac cfg 2 cw_ming 7 cw_max 15 aifs 2 txop 3008
[  459.260974] D:cmd configure (3)
[  459.264564] D:acx tid config
[  459.267594] D:cmd configure (9)
[  459.271476] D:mac80211 conf tx 2
[  459.274873] D:acx ac cfg 0 cw_ming 15 cw_max 1023 aifs 3 txop 0
[  459.281315] D:cmd configure (3)
[  459.284909] D:acx tid config
[  459.287939] D:cmd configure (9)
[  459.291791] D:mac80211 conf tx 3
[  459.295189] D:acx ac cfg 1 cw_ming 15 cw_max 1023 aifs 7 txop 0
[  459.301630] D:cmd configure (3)
[  459.305226] D:acx tid config
[  459.308258] D:cmd configure (9)
[  459.312112] D:mac80211 bss info role 0 changed 0x2000
[  459.317436] D:mac80211 config psm off power 0 idle changed 0xffffff9f
[  459.324486] D:mac80211 configure filter changed 180 total 80000180
wlan1: interface state UNINITIALIZED->COUNTRY_UP[  459.334607] cfg80211: Calling CRDA to update world regulatory domain
DATE
Add interface 'wlan1'
OK
###configure ip......................
[  459.350178] D:mac80211 configure filter changed 180 total 80000180
###start udhcpd server.............
[  459.369446] D:mac80211 configure filter changed 180 total 80000180
[  459.410233] D:elp work
[  459.412752] D:chip to elp

###configure nat.......................
root@am335x-evm:/usr/share/wl18xx# Using interface wlan1 with hwaddr 5c:31:3e:e1:a8:ac and ssid "SitaraAP"
[  460.368219] D:mac80211 config psm off power 0 in use changed 0x100
[  460.375299] D:waking up chip from elp
[  460.385141] D:wakeup time: 10 ms
[  460.388557] D:mac80211 add chanctx 11 (type 1)
[  460.393279] D:mac80211 assign chanctx (role 0) 11 (type 1) (radar 0 dfs_state 0)
[  460.401070] D:IRQ work
[  460.403685] D:intr: 0x20 (fw_rx_counter = 0, drv_rx_counter = 0, tx_results_counter = 0)
[  460.412220] D:WL1271_ACX_INTR_HW_AVAILABLE
[  460.416621] D:intr: 0x0 (fw_rx_counter = 0, drv_rx_counter = 0, tx_results_counter = 0)
[  460.425652] D:mac80211 bss info role 0 changed 0x40000
[  460.431253] D:acx dot11_cur_tx_pwr 20
[  460.435108] D:cmd configure (61)
[  460.438839] D:mac80211 bss info role 0 changed 0x4000
[  460.444524] D:mac80211 get tsf
[  460.447741] D:cmd interrogate
[  460.451429] D:mac80211 bss info role 0 changed 0x98360
[  460.456845] D:AP basic rate set: 0x26f
[  460.460813] D:acx ap rate policy 0 rates 0x26f
[  460.465636] D:cmd configure (27)
[  460.469655] D:acx ap rate policy 1 rates 0x1
[  460.474355] D:cmd configure (27)
[  460.478044] D:acx ap rate policy 2 rates 0x1ffeff
[  460.483231] D:cmd configure (27)
[  460.486920] D:acx ap rate policy 3 rates 0x1ffeff
[  460.492101] D:cmd configure (27)
[  460.495778] D:acx ap rate policy 4 rates 0x1ffeff
[  460.500953] D:cmd configure (27)
[  460.504630] D:acx ap rate policy 5 rates 0x1ffeff
[  460.509574] D:cmd configure (27)
[  460.513546] D:cmd template_set 16 (role 0)
[  460.518184] D:cmd template_set 0 (role 0)
[  460.522979] D:cmd template_set 5 (role 0)
[  460.527510] D:acx beacon filter opt enable=0
[  460.532230] D:cmd configure (11)
[  460.535921] D:cmd template_set 14 (role 0)
[  460.540852] D:probe response updated
[  460.544624] D:beacon updated
[  460.547651] D:cmd template_set 13 (role 0)
[  460.552631] D:beacon interval updated: 100
[  460.556948] D:cmd template_set 14 (role 0)
[  460.561926] D:probe response updated
[  460.565693] D:beacon updated
[  460.568719] D:cmd template_set 13 (role 0)
[  460.573779] D:cmd role start ap 0
[  460.577276] D:cmd role start ap with supported_rates 0x001ffeff
[  460.584822] D:started AP
[  460.587525] D:IRQ work
[  460.590114] D:intr: 0x40 (fw_rx_counter = 0, drv_rx_counter = 0, tx_results_counter = 0)
[  460.598622] D:WL1271_ACX_INTR_DATA
[  460.602282] D:intr: 0x0 (fw_rx_counter = 0, drv_rx_counter = 0, tx_results_counter = 0)
[  460.611596] D:mac80211 bss info role 0 changed 0x3e
[  460.616743] D:AP basic rate set: 0x26f
[  460.620741] D:acx ap rate policy 0 rates 0x26f
[  460.625661] D:cmd configure (27)
[  460.629773] D:acx ap rate policy 1 rates 0x1
[  460.634448] D:cmd configure (27)
[  460.638139] D:acx ap rate policy 2 rates 0x1ffeff
[  460.643324] D:cmd configure (27)
[  460.647008] D:acx ap rate policy 3 rates 0x1ffeff
[  460.652199] D:cmd configure (27)
[  460.655886] D:acx ap rate policy 4 rates 0x1ffeff
[  460.661061] D:cmd configure (27)
[  460.664746] D:acx ap rate policy 5 rates 0x1ffeff
[  460.669688] D:cmd configure (27)
[  460.673664] D:cmd template_set 16 (role 0)
[  460.678297] D:cmd template_set 0 (role 0)
[  460.683097] D:cmd template_set 5 (role 0)
[  460.687629] D:acx beacon filter opt enable=0
[  460.692348] D:cmd configure (11)
[  460.696039] D:cmd template_set 14 (role 0)
[  460.701010] D:probe response updated
[  460.704777] D:beacon updated
[  460.707809] D:cmd template_set 13 (role 0)
[  460.712855] D:acx slot
[  460.715345] D:cmd configure (2)
[  460.718918] D:acx_set_preamble
[  460.722439] D:cmd configure (30)
[  460.726082] D:acx_set_ctsprotect
[  460.729478] D:cmd configure (28)
[  460.733523] D:acx ht information setting
[  460.737649] D:cmd configure (49)
[  460.741944] D:mac80211 conf tx 0
[  460.745356] D:acx ac cfg 3 cw_ming 3 cw_max 7 aifs 1 txop 1504
[  460.751840] D:cmd configure (3)
[  460.755480] D:acx tid config
[  460.758513] D:cmd configure (9)
[  460.762415] D:mac80211 bss info role 0 changed 0x2000
[  460.767954] D:mac80211 conf tx 1
[  460.771393] D:acx ac cfg 2 cw_ming 7 cw_max 15 aifs 1 txop 3008
[  460.777832] D:cmd configure (3)
[  460.781875] D:acx tid config
[  460.784910] D:cmd configure (9)
[  460.788448] D:mac80211 bss info role 0 changed 0x2000
[  460.794274] D:mac80211 conf tx 2
[  460.797678] D:acx ac cfg 0 cw_ming 15 cw_max 63 aifs 3 txop 0
[  460.804021] D:cmd configure (3)
[  460.807646] D:acx tid config
[  460.810928] D:cmd configure (9)
[  460.814486] D:mac80211 bss info role 0 changed 0x2000
[  460.820273] D:mac80211 conf tx 3
[  460.823678] D:acx ac cfg 1 cw_ming 15 cw_max 1023 aifs 7 txop 0
[  460.829895] D:cmd configure (3)
[  460.833833] D:acx tid config
[  460.836868] D:cmd configure (9)
[  460.840724] D:mac80211 bss info role 0 changed 0x2000
wlan1: interface state COUNTRY_UPDATE->ENABLED
wlan1: AP-ENABLED
[  460.870015] D:elp work
[  460.872510] D:chip to elp