This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 EDMA LINK



DSP:C6678

CS5.3

hParamPing = CSL_edma3GetParamHandle(hChannel, ParamNum, &status);

hParamPing1 = CSL_edma3GetParamHandle(hChannel, ParamNum+3, &status)

myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPing1,0); // 这句话没有工作,并没有跳转到hParamPing1 所对应的PRAM;

  • 查看EDMA3的手册,然后找到你配置的对应寄存器地址,看看有没有正确的写下去。

    下面的代码供参考

    /* ===========================================================================
    * Copyright (c) Texas Instruments Inc 2002, 2003, 2004, 2005
    *
    * Use of this software is controlled by the terms and conditions found in the
    * license agreement under which this software has been supplied.
    * ==========================================================================
    */

    /** ===========================================================================
    *
    * @file Edma_ping_pong_xfer_gbl_reg.c
    *
    * @path $(CSLPATH)\example\edma\edma_ping_pong_xfer_gbl_reg\src
    *
    * @desc Example of EDMA
    *
    * ============================================================================
    * @n <b> Example Description </b>
    * @n This is an example of the CSL EDMA usage for the
    * Channel Initialization for ping pong buffer transfer
    * where channels are opened in the global region
    *
    *=============================================================================
    *
    * <b> Test Procedure </b>
    * @verbatim
    * 1. Configure the CCS setup to work with the emulator being used
    * 2. Please refer CCS manual for setup configuration and loading
    * proper GEL file
    * 3. Launch CCS window
    * 4. Open project Edma_ping_pong_xfer_gbl_reg.pjt
    * 5. Build the project and load the .out file of the project.
    * 6. The example can be executed from the main().
    *
    * @endverbatim
    *
    *
    * =============================================================================
    */

    /* ============================================================================
    * Revision History
    * ===============
    * 29-May-2004 Ruchika Kharwar File Created.
    *
    * ============================================================================
    */

    #include <stdio.h>
    #include <csl_edma3.h>
    #include <soc.h>

    /* Globals */
    Uint8 srcBuff1[256];
    Uint8 srcBuff2[256];
    Uint8 dstBuff1[256];
    Uint8 dstBuff2[256];
    Uint32 passStatus = 1;

    /* Forward declaration */
    void edma_ping_pong_xfer_gbl_region (void);

    /*
    * =============================================================================
    * @func main
    *
    * @desc
    * This is the main routine for the file.
    *
    * =============================================================================
    */
    void main(void)
    {

    /* Invoke example */
    edma_ping_pong_xfer_gbl_region ();

    return;
    }

    /*
    * =============================================================================
    * @func edma_ping_pong_xfer_gbl_region
    *
    * @arg
    * NONE
    *
    * @desc
    * This is the example routine which perform edma ping pong buffer transfer
    * where channel is open in the global region.
    *
    * @return
    * NONE
    *
    * =============================================================================
    */
    void edma_ping_pong_xfer_gbl_region (void)
    {
    CSL_Edma3Handle hModule;
    // CSL_Edma3HwSetup hwSetup;
    CSL_Edma3Obj edmaObj;
    CSL_Edma3ParamHandle hParamPing;
    CSL_Edma3ParamHandle hParamPong;
    CSL_Edma3ParamHandle hParamBasic;
    CSL_Edma3ChannelObj chObj;
    CSL_Edma3CmdIntr regionIntr;
    CSL_Edma3ChannelHandle hChannel;
    CSL_Edma3ParamSetup myParamSetup;
    CSL_Edma3Context context;
    CSL_Edma3ChannelAttr chAttr;
    CSL_Status status;
    // CSL_Edma3HwDmaChannelSetup dmahwSetup;
    Uint32 loopIndex;


    /* Initialize data */
    for (loopIndex = 0; loopIndex < 256; loopIndex++) {
    srcBuff1[loopIndex] = loopIndex;
    srcBuff2[loopIndex] = loopIndex;
    dstBuff1[loopIndex] = 0;
    dstBuff2[loopIndex] = 0;
    }

    /* Module initialization */
    status = CSL_edma3Init(&context);
    if (status != CSL_SOK) {
    printf ("Edma module initialization failed\n");
    return;
    }

    /* Module level open */
    hModule = CSL_edma3Open(&edmaObj,CSL_EDMA3,NULL,&status);
    if ( (hModule == NULL) || (status != CSL_SOK)) {
    printf ("Edma module open failed\n");
    return;
    }
    #if 0
    /* Module setup */
    dmahwSetup.paramNum = 0;
    dmahwSetup.que = CSL_EDMA3_QUE_0;
    hwSetup.dmaChaSetup = &dmahwSetup;
    hwSetup.qdmaChaSetup = NULL;
    status = CSL_edma3HwSetup(hModule,&hwSetup);
    if (status != CSL_SOK) {
    printf ("Hardware setup failed\n");
    CSL_edma3Close (hModule);
    return;
    }
    #endif
    /* Channel open */
    chAttr.regionNum = CSL_EDMA3_REGION_GLOBAL;
    chAttr.chaNum = CSL_EDMA3_CHA_TEVTLO0;
    hChannel = CSL_edma3ChannelOpen(&chObj, CSL_EDMA3, &chAttr, &status);
    if ((hChannel == NULL) || (status != CSL_SOK)) {
    printf ("Edma channel open failed\n");
    return;
    }

    CSL_edma3HwChannelSetupParam(hChannel, CSL_EDMA3_CHA_TEVTLO0);
    if (status != CSL_SOK) {
    printf ("Edma channel setup param failed\n");
    return;
    }

    /* Change Channel Default queue setup from 0 to 3 */
    status = CSL_edma3HwChannelSetupQue(hChannel,CSL_EDMA3_QUE_3);
    if (status != CSL_SOK) {
    printf ("Edma channel setup que failed\n");
    return;
    }

    /* Obtain a handle to parameter set 0 */
    hParamBasic = CSL_edma3GetParamHandle(hChannel,0,NULL);
    if (hParamBasic == NULL) {
    printf ("Edma get param handle for param entry 0 failed\n");
    return;
    }

    /* Obtain a handle to parameter set 2 */
    hParamPing = CSL_edma3GetParamHandle(hChannel,2,NULL);
    if (hParamPing == NULL) {
    printf ("Edma get param handle for param entry 2 failed\n");
    return;
    }

    /* Obtain a handle to parameter set 1 */
    hParamPong = CSL_edma3GetParamHandle(hChannel,1,NULL);
    if (hParamPong == NULL) {
    printf ("Edma get param handle for param entry 1 failed\n");
    return;
    }

    /* Setup the parameter entry parameters (Ping buffer) */
    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
    CSL_EDMA3_TCCH_DIS, \
    CSL_EDMA3_ITCINT_DIS, \
    CSL_EDMA3_TCINT_EN, \
    0,CSL_EDMA3_TCC_NORMAL,\
    CSL_EDMA3_FIFOWIDTH_NONE, \
    CSL_EDMA3_STATIC_DIS, \
    CSL_EDMA3_SYNC_A, \
    CSL_EDMA3_ADDRMODE_INCR, \
    CSL_EDMA3_ADDRMODE_INCR );
    myParamSetup.srcAddr = (Uint32)srcBuff1;
    myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(256,1);
    myParamSetup.dstAddr = (Uint32)dstBuff1;
    myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,1);
    myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);
    myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);
    myParamSetup.cCnt = 1;
    status = CSL_edma3ParamSetup(hParamBasic,&myParamSetup);
    if (status != CSL_SOK) {
    printf("Edma parameter entry setup is failed\n");
    return;
    }

    /* Ping setup */
    status = CSL_edma3ParamSetup(hParamPing,&myParamSetup);
    if (status != CSL_SOK) {
    printf("Edma ping parameter entry setup is failed\n");
    return;
    }

    /* Pong setup */
    myParamSetup.linkBcntrld = CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPing,0);
    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
    CSL_EDMA3_TCCH_DIS, \
    CSL_EDMA3_ITCINT_DIS, \
    CSL_EDMA3_TCINT_EN,\
    1,CSL_EDMA3_TCC_NORMAL,\
    CSL_EDMA3_FIFOWIDTH_NONE, \
    CSL_EDMA3_STATIC_EN, \
    CSL_EDMA3_SYNC_A, \
    CSL_EDMA3_ADDRMODE_INCR, \
    CSL_EDMA3_ADDRMODE_INCR );
    myParamSetup.srcAddr = (Uint32)srcBuff2;
    myParamSetup.dstAddr = (Uint32)dstBuff2;
    status = CSL_edma3ParamSetup(hParamPong,&myParamSetup);
    if (status != CSL_SOK) {
    printf("Edma ping parameter entry setup is failed\n");
    return;
    }

    /* Interrupt enable (Bits 0-1) for the global region interrupts */
    regionIntr.region = CSL_EDMA3_REGION_GLOBAL ;
    regionIntr.intr = 0x3 ;
    regionIntr.intrh = 0x0000 ;
    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTR_ENABLE,&regionIntr);

    /* Trigger channel */
    CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);
    regionIntr.region = CSL_EDMA3_REGION_GLOBAL ;
    regionIntr.intr = 0 ;
    regionIntr.intrh = 0 ;

    /* Poll on IPR bit 0 */
    do {
    CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);
    } while (!(regionIntr.intr & 0x1));

    /* Clear the pending bit */
    CSL_edma3HwControl(hModule,CSL_EDMA3_CMD_INTRPEND_CLEAR,&regionIntr);

    /* Trigger Channel */
    CSL_edma3HwChannelControl(hChannel,CSL_EDMA3_CMD_CHANNEL_SET,NULL);

    /* Poll on IPR bit 2 */
    do {
    CSL_edma3GetHwStatus(hModule,CSL_EDMA3_QUERY_INTRPEND,&regionIntr);
    } while (!(regionIntr.intr & 0x2));

    /* Check transfer by comparing the source and destination buffers */
    if(Verify_Transfer( 256, 1, 1, 0, 0, 0, 0, srcBuff1, dstBuff1, \
    TRUE) == FALSE)
    passStatus = 0;

    if(Verify_Transfer( 256, 1, 1, 0, 0, 0, 0, srcBuff2, dstBuff2, \
    TRUE) == FALSE)
    passStatus = 0;

    if (passStatus == 1)
    printf ("<<EXAMPLE PASSED>>: Edma Ping Pong Buffer Transfer Passed\n");
    else {
    printf ("<<EXAMPLE FAILED>>: Edma Ping Pong Buffer Transfer Failed\n");
    return;
    }

    /* Close channel */
    status = CSL_edma3ChannelClose(hChannel);
    if (status != CSL_SOK) {
    printf("Edma channel close failed\n");
    return;
    }

    /* Close edma module */
    status = CSL_edma3Close(hModule);
    if (status != CSL_SOK) {
    printf("Edma module close failed\n");
    return;
    }

    printf ("=============================================================\n");

    return;
    }

  • 谢答!这几天把技术手册看了一下,感觉还是需要看懂技术手册,应为挺重要的。

    myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
    CSL_EDMA3_TCCH_DIS, \
    CSL_EDMA3_ITCINT_DIS, \
    CSL_EDMA3_TCINT_EN, \
    0,CSL_EDMA3_TCC_NORMAL,\
    CSL_EDMA3_FIFOWIDTH_NONE, \
    CSL_EDMA3_STATIC_DIS, \
    CSL_EDMA3_SYNC_A, \
    CSL_EDMA3_ADDRMODE_INCR, \
    CSL_EDMA3_ADDRMODE_INCR );


    这个都参数挺重要。看懂一下,还是TCC寄存器得看明白