This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 上运行OpneMp 例程出问题,请求专家帮助。



   最近在做C6678这块,由于内存需求比较大,外接了8个G的内存,目前暂时使用2个G。算法打算采用OpenMp的方式进行多核并行,创建了一个OpenMp的例子工程 OpenMp Matri vector,完全按照它的东西运行是没有问题的。但是我需要使用2G的内存,修改它自带的RTSC内存配置,增加额外的内存 MSMCSRAM_CACHE,当MSMCSRAM_CACHE 长度为0x10000000时,结果也是正常的;当MSMCSRAM_CACHE长度为0x20000000或者其他大于0x10000000长度的,多核就跑飞了。

    

   

       MSMCSRAM_CACHE存储段只是定义了,在工程里面没有使用到,既然没有使用到怎么会飞掉呢。我想问下是不是对于OpenMp的例子它配套的RTSC存储段的配置是不是在它的内核里面做了限制不能修改,不能增加额外的内存。对于OpenMp的内存配置除了增加这里,还需要在其他的地方设置。

     请TI的专家帮我解答下,谢谢。