This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: Main CPSW RGMII not work issue

Part Number: DRA821U


Dear TI,

We made a new board with J7200(DRA821U), and use sdk "ti-processor-sdk-linux-j7200-evm-09_02_00_05".

The board have three ethernet ports, one mcu_cpsw, and two ports on Main CPSW.

For now, mcu_cpsw already work normal, but main cpsw ports not work, we used mofiled the dtso file "k3-j7200-evm-quad-port-eth-exp.dtso" as below, which already disabled unused port3 and port4

/dts-v1/;                                                                                                                                                                                                                                                     
/plugin/;                                                                                                                                                                                                                                                     
                                                                                                                                                                                                                                                              
#include <dt-bindings/gpio/gpio.h>                                                                                                                                                                                                                            
#include <dt-bindings/mux/ti-serdes.h>                                                                                                                                                                                                                        
#include <dt-bindings/net/ti-dp83867.h>                                                                                                                                                                                                                       
                                                                                                                                                                                                                                                              
#include "k3-pinctrl.h"                                                                                                                                                                                                                                       
                                                                                                                                                                                                                                                              
&{/} {                                                                                                                                                                                                                                                        
        aliases {                                                                                                                                                                                                                                             
                ethernet1 = "/bus@100000/ethernet@c000000/ethernet-ports/port@1";                                                                                                                                                                             
                ethernet2 = "/bus@100000/ethernet@c000000/ethernet-ports/port@2";                                                                                                                                                                             
                //ethernet3 = "/bus@100000/ethernet@c000000/ethernet-ports/port@3";                                                                                                                                                                           
                //ethernet4 = "/bus@100000/ethernet@c000000/ethernet-ports/port@4";                                                                                                                                                                           
        };                                                                                                                                                                                                                                                    
};                                                                                                                                                                                                                                                            
                                                                                                                                                                                                                                                              
&cpsw0 {                                                                                                                                                                                                                                                      
        status = "okay";                                                                                                                                                                                                                                      
};                                                                                                                                                                                                                                                            
                                                                                                                                                                                                                                                              
&cpsw0_port1 {                                                                                                                                                                                                                                                
        status = "okay";                                                                                                                                                                                                                                      
        phy-handle = <&cpsw5g_phy0>;                                                                                                                                                                                                                          
        phy-mode = "qsgmii";                                                                                                                                                                                                                                  
        mac-address = [00 00 00 00 00 00];                                                                                                                                                                                                                    
        phys = <&cpsw0_phy_gmii_sel 1>;                                                                                                                                                                                                                       
};                                                                                                                                                                                                                                                            
                                                                                                                                                                                                                                                              
&cpsw0_port2 {                                                                                                                                                                                                                                                
        status = "okay";                                                                                                                                                                                                                                      
        phy-handle = <&cpsw5g_phy1>;                                                                                                                                                                                                                          
        phy-mode = "qsgmii";                                                                                                                                                                                                                                  
        mac-address = [00 00 00 00 00 00];                                                                                                                                                                                                                    
        phys = <&cpsw0_phy_gmii_sel 2>;                                                                                                                                                                                                                       
};                                                                                                                                                                                                                                                            
                                                                                                                                                                                                                                                              
&cpsw0_port3 {                                                                                                                                                                                                                                                
        status = "disabled";                                                                                                                                                                                                                                  
        phy-handle = <&cpsw5g_phy2>;                                                                                                                                                                                                                          
        phy-mode = "qsgmii";                                                                                                                                                                                                                                  
        mac-address = [00 00 00 00 00 00];                                                                                                                                                                                                                    
        phys = <&cpsw0_phy_gmii_sel 3>; 
};

&cpsw0_port4 {
        status = "disabled";
        phy-handle = <&cpsw5g_phy3>;
        phy-mode = "qsgmii";
        mac-address = [00 00 00 00 00 00];
        phys = <&cpsw0_phy_gmii_sel 4>;
};

&cpsw5g_mdio {
        status = "okay";
        pinctrl-names = "default";
        pinctrl-0 = <&mdio0_pins_default>;
        //reset-gpios = <&exp2 17 GPIO_ACTIVE_LOW>;
        //reset-post-delay-us = <120000>;
        #address-cells = <1>;
        #size-cells = <0>;

        cpsw5g_phy0: ethernet-phy@0 {
                reg = <0>;
                ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
                ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
        };
        cpsw5g_phy1: ethernet-phy@1 {
                reg = <1>;
                ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_00_NS>;
                ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
        };
        cpsw5g_phy2: ethernet-phy@18 {
                reg = <18>;
        };
        cpsw5g_phy3: ethernet-phy@19 {
                reg = <19>;
        };
};

/*
&exp2 {
        qsgmii-line-hog {
                gpio-hog;
                gpios = <16 GPIO_ACTIVE_HIGH>;
                output-low;
                line-name = "qsgmii-pwrdn-line";
        };
};
*/

&main_pmx0 {
        mdio0_pins_default: mdio0-pins-default {
                pinctrl-single,pins = <
                        J721E_IOPAD(0x00a8, PIN_OUTPUT, 5) /* (W19) UART8_TXD.MDIO0_MDC */
                        J721E_IOPAD(0x00a4, PIN_INPUT, 5) /* (W14) UART8_RXD.MDIO0_MDIO */
                >;
        };
};

and we can see the eth0(mcu_cpsw) and eth1, eth2 on main cpsw by ifconfig command.

root@j7200-evm:~# ifconfig
eth0      Link encap:Ethernet  HWaddr 58:A1:5F:BE:63:2B
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

eth1      Link encap:Ethernet  HWaddr 2E:5A:03:A5:9C:F0
          inet addr:192.168.1.10  Bcast:192.168.1.255  Mask:255.255.255.0
          inet6 addr: fe80::2c5a:3ff:fea5:9cf0/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:104 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:11261 (10.9 KiB)

eth2      Link encap:Ethernet  HWaddr 8E:D0:AF:A7:9F:41
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:192 errors:0 dropped:0 overruns:0 frame:0
          TX packets:192 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:18456 (18.0 KiB)  TX bytes:18456 (18.0 KiB)

however, after set ip for eth1 or eth2, it ping failed, and print lots of logs as below.

[ 1977.825539] am65-cpsw-nuss c000000.ethernet eth1: txq:0 DRV_XOFF:0 tmo:1404352 dql_avail:-39 free_desc:505
[ 1982.945537] am65-cpsw-nuss c000000.ethernet eth1: txq:0 DRV_XOFF:0 tmo:1409472 dql_avail:-39 free_desc:505
[ 1988.065539] am65-cpsw-nuss c000000.ethernet eth1: txq:0 DRV_XOFF:0 tmo:1414592 dql_avail:-39 free_desc:505
[ 1994.209536] am65-cpsw-nuss c000000.ethernet eth1: txq:0 DRV_XOFF:0 tmo:1420736 dql_avail:-39 free_desc:505

I have tried to change "phy-mode" to "rgmii", "rgmii-rxid", "rgmii-id", but not work.

attach the dmesg log on boot as below.

root@j7200-evm:~# dmesg |grep ether
[    0.954049] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    0.954145] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    0.954148] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    0.954583] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[    0.993237] am65-cpsw-nuss c000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 5 quirks:00000000
[    0.993322] am65-cpsw-nuss c000000.ethernet: Use random MAC address
[    0.993379] am65-cpsw-nuss c000000.ethernet: Use random MAC address
[    0.993388] am65-cpsw-nuss c000000.ethernet: initialized cpsw ale version 1.4
[    0.993391] am65-cpsw-nuss c000000.ethernet: ALE Table size 512
[    0.993696] am65-cpsw-nuss c000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[    1.062112] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[    1.062206] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[    1.062209] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[    1.062596] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[    1.089015] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[    1.130501] am65-cpsw-nuss c000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 5 quirks:00000000
[    1.130613] am65-cpsw-nuss c000000.ethernet: Use random MAC address
[    1.130670] am65-cpsw-nuss c000000.ethernet: Use random MAC address
[    1.130679] am65-cpsw-nuss c000000.ethernet: initialized cpsw ale version 1.4
[    1.130682] am65-cpsw-nuss c000000.ethernet: ALE Table size 512
[    1.130979] am65-cpsw-nuss c000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[    1.157241] am65-cpsw-nuss c000000.ethernet: set new flow-id-base 60
[    4.680095] am65-cpsw-nuss c000000.ethernet: PSI-L request err -22
[    4.742143] am65-cpsw-nuss c000000.ethernet eth2: PHY [c000f00.mdio:01] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[    4.742157] am65-cpsw-nuss c000000.ethernet eth2: configuring for phy/qsgmii link mode
[    4.821078] am65-cpsw-nuss c000000.ethernet eth1: PHY [c000f00.mdio:00] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[    4.821092] am65-cpsw-nuss c000000.ethernet eth1: configuring for phy/qsgmii link mode
[    4.903243] am65-cpsw-nuss 46000000.ethernet eth0: PHY [46000f00.mdio:02] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[    4.903257] am65-cpsw-nuss 46000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[    8.930592] am65-cpsw-nuss c000000.ethernet eth1: Link is Up - 1Gbps/Full - flow control rx/tx

we can see the error message "[    4.680095] am65-cpsw-nuss c000000.ethernet: PSI-L request err -22" , but don't know why.

For this issue, how can I check next?

BR 

guangtao