大家好,我手头有批8148的板子,目前测试发现DDR颗粒焊接有问题,所以我把DDR颗粒拆了,现在 8148的电源、外部晶振始终正常的,请问还能通过测试哪些信号来判断此时的8148可正常,目前板子还有外设如下:
1、SD卡
2、SPI FLASH;
3、NAND FLASH;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我手头有批8148的板子,目前测试发现DDR颗粒焊接有问题,所以我把DDR颗粒拆了,现在 8148的电源、外部晶振始终正常的,请问还能通过测试哪些信号来判断此时的8148可正常,目前板子还有外设如下:
1、SD卡
2、SPI FLASH;
3、NAND FLASH;
你好,
配置为uart启动,看串口是否有打印,uboot min是否能下载成功(运行应该是有问题,因为没有DDR)。
设置SPI启动,串口打印“CCCCCCCC”;
设置串口启动,串口打印“CCCCCCCC”;
我们用仿真器连接JTAG口,能连上仿真器,但是U-BOOT下载不成功
你好,
有CCC,能基本说明芯片已经正常启动了(ROM code).
抱歉,只有DM816x uboot里面有支持只在ocmc运行的uboot min。DM814x上是没有的。
DM816x的相关信息可以参考:http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/p/44813/97852.aspx