This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to use Host descriptor for AIF2 CPRI and LTE FDD Mode?



I want use host descriptor for CPRI and LTE FDD mode.

But example for LTE FDD mode in PDK used monolithic descriptor, and host is only useddescriptor for generic packet mode in AIF diver provided by PDK

 

Can I just modify PKTDMA configuration based on LTE FDD mode example?

 

Word 3 in monolithic descriptor includes AXC number and symbol number, how can I set for host descriptor?

  • 正常情况下AIF要使用mono的描述符,主要是出于对访问效率的考虑,使用mono的描述符pktdma可以一次就获取到数据的地址信息,而使用host descriptor,pktdma要解析buffer指针才能获取数据地址,而CPRI是严格时钟同步的接口,当流量比较大的时候有可能会影响CPRI的传输。

    如果你要使用host descriptor,直接初始化好push到队列里即可,没有特殊操作。

  • Mono模式的描述符word 3中,携带了AXC序号和symbol的序号,我理解AIF FDD LTE模式时,是在10ms帧的开始从symbol 0到symbol 139依次发送的;

    Host模式不知道有没有设置这些的地方,如果没有设置会不会有问题?