最近在调试6455 DSP flash加载功能,一直不成功。
今天用示波器抓了下上电时刻CE3片选对flash读数据波形(CE3,OE,DATA0),发现emif总线只读了大约200个字节数据就不变了。
如果flash里烧写的boot代码都00,,emif总线读了大约1K字节数据才不变了。
请问 dsp上电时,通过EDMA搬移flash内的1K数据到内部RAM,这个过程有可能被打断吗?dsp是在搬移完1K代码后才开始运行代码,还是边搬移边运行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在调试6455 DSP flash加载功能,一直不成功。
今天用示波器抓了下上电时刻CE3片选对flash读数据波形(CE3,OE,DATA0),发现emif总线只读了大约200个字节数据就不变了。
如果flash里烧写的boot代码都00,,emif总线读了大约1K字节数据才不变了。
请问 dsp上电时,通过EDMA搬移flash内的1K数据到内部RAM,这个过程有可能被打断吗?dsp是在搬移完1K代码后才开始运行代码,还是边搬移边运行?
从EMIFA boot时,如下:
2.3.3 EMIFA Boot Mode
In EMIFA boot mode, the bootloader simply branches to the base address of EMIFA CE3 (0xB000 0000).
Interrupts are disabled.
因此不存在1K的规定,这点和C6713不同。在EMIFA CE3 (0xB000 0000)这个位置应该存放的二次bootloader,一次搬运完成后,然后才把控制权交给DSP,然后在内存中开始运行二次bootloader。