This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320C6713BZDP300 芯片,工作在300MHZ时需要1.4V内核电压(CVDD),现在想让他替代TMS320C6713BZDP225,只需要工作在 225MHZ频率,那么内核电压(CVDD)是否可以用1.2V?
还是用1.4v比较保险,请看下面的回复。
I just heard back from manufacturing. They indicate that 1.4V 300MHz devices are only tested to datasheet speeds at 1.4V -- there is no 100% guarantee that the -300 devices will operate at 225MHz at 1.2V. Personally, I think it should be fine using -300 devices for 1.2V/225MHz, but the customer needs to understand that they are using the drop-in replacement at their own risk.