This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DM8127的ISP 2A算法如何配置?



我们最近打算在DM8127的IPNC RDK3.8上调试ISP的2A算法,现在已经跑通了raw data的case但是发现有个问题:在RDK的每一帧回调函数Iss_ispDrvCallBack里并没有调用IssAlg_capt2AIsrCallBack(pObj->p2AObj) 这个函数,这样说明RDK是不是默认不使能ISP的2A算法?如果没使能2a算法我们应该如何配置RDK?

  • Aen,

    你是如何判断Iss_ispDrvCallBack里并没有调用IssAlg_capt2AIsrCallBack(pObj->p2AObj) 这个函数你是有在下面函数加打印发现ISPDRV_ENABLE_2A_ISP没有定义么?

    默认IPNC的2A是开启的,注意IE界面是可以关闭2A的。

    Int32 Iss_ispDrvCallBack()
    {
    ...

    #ifdef ISPDRV_ENABLE_2A_ISP
                IssAlg_capt2AIsrCallBack(pObj->p2AObj);
    #endif

  • hi:

    Chris

    我有在RDK3.8下面函数加打印发现ISPDRV_ENABLE_2A_ISP没有定义

    Int32 Iss_ispDrvCallBack()
    {
    ...

    #ifdef ISPDRV_ENABLE_2A_ISP
                IssAlg_capt2AIsrCallBack(pObj->p2AObj);
    #endif

    另外我搜了RDK的代码没有ISPDRV_ENABLE_2A_ISP这个宏的定义