This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM36X 配2G比特DDR2的问题



Hi:

  大家好,新做的DM36X+ 2G DDR2板子, 分别贴了10片DM365, 10片DM368芯片的板子。 在UBL代码的 Uint32 DEVICE_DDR2Init() 里面修改了一下页大小,从1024改成2048.

     目前用DM365 编译的UBL, UBOOT 可以在DM365的板子正常工作;

     用DM368编译的UBL,UBOOT在DM368的板子烧录后,启动板子后如下提示:

DM36x initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000008.
   DONE
Jumping to 22 entry point at 0x81080000.

 DM368_IPNC_UBL_1.0.1

 卡在这里不动了, UBL, UBOOT 我们还是用的V2.5的版本, 查了一下V5.1的版本的UBL DDR2初始化哪里改了一点时序, 现在不知道是否板子DDR2 LAYOUT 问题 还是 UBL,UBOOT代码问题?  有谁碰过这个问题吗?

谢谢