This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI FLASH boot 在EVM6678上不成功



1 启动模式设置spi 模式,sw3 1 1 0 1 ,但是识别是1 0 1 1 ,也就是识别成i2c模式 ,不知道为什么

2 假设 能识别spi模式,6678rom自己会从spi flash加载数据到执行地址?????

  • 查看DEVSTAT寄存器值,check对应的boot mode;

    SPI模式支持norflash加载,根据boot pin配置进行SPI配置及加载。具体参考6678 RBL SPI加载流程。

    http://processors.wiki.ti.com/index.php/Keystone_Device_Architecture

  • 1 现在spi启动,从读出的数据来看总是第一个字节,这是配置4pin

    2 我要是配5pin,数据线变化的比时钟线快,读出的数据也不对

    我们的这个板有两个片选,一个访问能n25q032的,一个是控制FPGA的spiflash的。